• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56304 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • kltm
    kltm over 6 years ago

    I’m pretty sure I could lay this out, I have CAD experience.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kltm

    I'll post a quick blog with the details about sizes of bits that I have and ideas re. boxes in the next few days.

    To get you started,

    the display I suggest (which costs about £30) is a high resolution 4.3" non touch with a built in high level controller.

    The capacity for controls is limited - I'm thinking 1 rotary and 4 buttons.

    The tricky stuff to work out is what standard box to start with - my first thought was a bit pricey at over £30,

    what level of environmental protection, how to install the battery, where the connectors go.

    Then how to attach the pcb and display to the box so you can see the display but water doesn't get in etc.

     

    In a brainstormy way I'm thinking,

     

    plastic box rated IP66, about 9" x 6" x 3"

    top held on by screws (often from back so you can't see them)

    space inside for 2 batteries so you only need to open the box every two days of work to change them

    otherwise some kind of battery door or maybe have them hanging on the outside like a camera

    protect the display with 2mm thick acrylic or polycarbonate

    use IP66 or better rated push buttons but the price is dreadful.

    no good ideas about how to seal the shaft or the rotary control, you could use one of those lovely Chinese CNC encoder wheels

    (about £15) which are surface mounted, but a bit big and pricey.

    The usual little Alps 6mm shaft job would need O rings and a bush

     

    Slightly away from mechanical I saw this (after John Wiltrout's scope repair post):

    http://www.hantek.com.cn/products/detail/16176

    The display is a knock off of the Keysight 34465A34465A but quite lovely. Our display is as good as that and it would be nice

    if anyone feels up to designing and coding an interface of that standard (but controlled by one rotary control and 4 buttons !)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 6 years ago in reply to kltm

    I'll post a quick blog with the details about sizes of bits that I have and ideas re. boxes in the next few days.

    To get you started,

    the display I suggest (which costs about £30) is a high resolution 4.3" non touch with a built in high level controller.

    The capacity for controls is limited - I'm thinking 1 rotary and 4 buttons.

    The tricky stuff to work out is what standard box to start with - my first thought was a bit pricey at over £30,

    what level of environmental protection, how to install the battery, where the connectors go.

    Then how to attach the pcb and display to the box so you can see the display but water doesn't get in etc.

     

    In a brainstormy way I'm thinking,

     

    plastic box rated IP66, about 9" x 6" x 3"

    top held on by screws (often from back so you can't see them)

    space inside for 2 batteries so you only need to open the box every two days of work to change them

    otherwise some kind of battery door or maybe have them hanging on the outside like a camera

    protect the display with 2mm thick acrylic or polycarbonate

    use IP66 or better rated push buttons but the price is dreadful.

    no good ideas about how to seal the shaft or the rotary control, you could use one of those lovely Chinese CNC encoder wheels

    (about £15) which are surface mounted, but a bit big and pricey.

    The usual little Alps 6mm shaft job would need O rings and a bush

     

    Slightly away from mechanical I saw this (after John Wiltrout's scope repair post):

    http://www.hantek.com.cn/products/detail/16176

    The display is a knock off of the Keysight 34465A34465A but quite lovely. Our display is as good as that and it would be nice

    if anyone feels up to designing and coding an interface of that standard (but controlled by one rotary control and 4 buttons !)

     

    MK