• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 55982 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • genebren
    genebren over 6 years ago

    Interesting ideas so far.  I meant to chime in earlier, but things have been pretty busy for me lately (building a deck and entertaining my Grandchildren again).

     

    Several years ago, I was asked to sit in with some friends of my sister that work at a geotech company.  They were looking to build impedance measurement devices for soil surveys.  I came across this amazing looking chip from Analog Devices that looked like a great way to measure impedance (including a complex component).

     

    Here is a snippet from the specification:

     

    The AD5934 is a high precision impedance converter system solution that combines an on-board frequency generator with a 12-bit, 250 kSPS, analog-to-digital converter (ADC). The frequency generator allows an external complex impedance to be excited with a known frequency. The response signal from the impedance is sampled by the on-board ADC and a discrete Fourier transform (DFT) is processed by an on-board DSP engine. The DFT algorithm returns a real (R) and imaginary (I) data-word at each output frequency.Once calibrated, the magnitude of the impedance and relative phase of the impedance at each frequency point along the sweep is easily calculated using the following two equations:Magnitude = 22IR+Phase = tan−1(I/R) A similar device, available from Analog Devices, Inc., is the AD5933, which is a 2.7 V to 5.5 V, 1 MSPS, 12-bit impedance converter, with an internal temperature sensor, available in a  16-lead SSOP.

     

     

    This might be of some help in your planning.

     

    Good luck and let me know if you need any help on this project.

     

     

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to genebren

    Hi Gene,

     

    It's a super-interesting chip, I was keen to use it a few years ago for plant soil purposes, and for hydroponics - to try to see if the soil or liquid has nutrients. The idea being to have a signature of known good soil or water by sweeping through the spectrum. I never got to try it though sadly, the project moved on to something else.

    It was felt that it could have had a lot of merit because then you could publish the signature, so others could try to replicate a yield (it wasn't going to be for farmers, more for home use), and to not waste nutrient. But, I have no idea in practice if the result would have been usable, or too inconsistent/variable.

    I wish I'd done some work on it at the time, since it could have been useful for other purposes too.

     

    The proposed design so far is one half of the impedance measuring system, but with digital processing. In theory it could be converted to an impedance measuring system with no additional hardware change, just a software upgrade, since the frequency will be know, and there will be some sync pulse from the FPGA, we just need to internally multiply with a 90 degree out of phase signal from that sync pulse too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to davemartin

    I am curious why it is important to get the same results.  The results change according to the moisture in the ground, where the stakes are placed, all sorts of stuff.  The important thing is to map the underground which this more sensitive circuit with the ability to change frequency and waveform should do better.

     

    Besides if it is so different that should get rid of all the complaints about copying ;-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • davemartin
    davemartin over 6 years ago in reply to paul_d_arch

    Paul, Mike, Shaz et al:

    paul_d_arch  wrote:

    ...The problem is - as you have said - is you have no experience of using this equipment in a wet field and those who have (may not have any electronics experience)  are telling you about the commercial equipment they are using....

    just to explain where I'm coming from - Physics first degree, then microelectronics. Career in IT then rugged embedded electronics, including designing carrier-phase GPS, inertial nav, high-vibration-deployed kit, etc. Long term archaeologist, arch geophys for at least 20 years.

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • paul_d_arch
    paul_d_arch over 6 years ago in reply to fmilburn

    Frank,

     

    Copying may have been was the wrong word - duplicating/replicating  may have been better. You have a valid point, why not take advantage of new technology to move forward.

     

    The 137Hz is, I suspect, a leftover artefact from the1920's and early hand wound equipment. There is a mathematical reason for 137 but the need for it may have long gone or other frequencies may be better suited to modern equipment.

     

    Paul D

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davemartin
    davemartin over 6 years ago in reply to paul_d_arch

    137Hz reversal is, I believe, chosen to be the lowest frequency that is clear of 50Hz and 60Hz mains and their harmonics, that gives just long enough in most cases to take a reading. Higher reversal rate negligible or no benefit for most use cases.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to davemartin

    Hi Dave,

     

    It can be demonstrated with (say) MATLAB. I'm tied up today, but it's possible to show that when switched at the source frequency, this is a mixing or multiplying action, and you end up with a steady fixed value measurement, regardless of sine or square excitation. The only difference is that there is more non-DC content to filter off with square excitation.

    Although it seems to be a DC measurement, it isn't, it is a very slow AC measurement that can be (sometimes) better understood as DC, but when looking at it from how it is measured, it can be seen it really is AC.

    I have a test instrument that uses square wave excitation. However I have another test instrument that uses a sine wave. Both provide similar results (almost near-identical, because they are both well-designed instruments). Both use averaging.

     

    In any case, it can be tested for real too. The proposed design can handle the square wave and synchronised measurement method, i.e. there's no hardware difference to do either method.

    The sine-wave method can be tested to see if it makes any difference, good or bad.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davemartin
    davemartin over 6 years ago in reply to fmilburn

    Frank,

     

    There's no doubt that AC excitation will produce results of some kind, and may even reveal something different to current techniques.

     

    The reason for maintaining continuity is that the physics is (relatively!) well understood and that current processing software can deal with it (particularly if inverting a many-probe section).

     

    Crucially though we need to consider why such equipment is used - it is not just to say "there's an anomaly in that part of the field", the plots are interpreted to try and postulate what may be beneath the soil. That is done on the basis of experience and by reference to known plots which have been ground-truthed (i.e. survey with a particular technique and then excavated).

     

    So, for general archaeological fieldwork it needs to use the same measurement principles.

     

    Alternative excitation strategies could well be an interesting research project but would not be relevant for those who, like Mr MacDonald who made the original posting, were looking for a more usable version of a low-cost instrument.

     

    Dave

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to davemartin

    In any case, the design supports the same square-wave method.

    There's no hardware cost or effort difference, which is good.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • davemartin
    davemartin over 6 years ago in reply to shabaz

    Thanks great Shabaz, what worried me was that a recent message said "the intent is to use sine waves",

    cheers

    Dave

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to davemartin

    I thought it might be helpful to followers of this thread to walk through the operation of the synchronous detector concept used in the Robert Beck design.

    This can be done with the aid of LTSpice (which is a free download from www.analog.com).

    I'll follow it up with a similar modelling of a phase sensitive detector -  which works on sine waves, and explain why any differences in results are all to the good of the PSD.

    As every one seems to agree: we are using AC because of electrolysis problems with DC, and we have to have some way of removing interference signals

    which are commonly at mains frequency and harmonics.

     

    image

    This is a reasonable model of the key parts of the synchronous rectifier in the Beck design.

     

     

    image

    I've given it a nice friendly input of a 1V pk sine wave at 50Hz (to represent interference) and a +/- 5V

    square wave for the signal. The signal frequency is not quite 137Hz. The node on the schematic is

    labelled IN

     

    image

    This is the signal at UNF (for unfiltered) and is what you get once the modulator has done its work. The

    spikes are caused by the finite switching speed of the FETs and amplifier. (We'll come back to them later.)

     

    image

    And final the output of the filter - on the Beck design this goes to a digital DC voltmeter and you record the reading

    by hand. Note the different scale.

     

    The filter has made a good job of getting rid of the AC components and the output is very close to what we would hope.

     

    There are some important points to note:

    1) the unfiltered signal never 'settles' because it has chopped up bits of the 50Hz interference added to it.

    2) in real life the interference signal may be larger than the wanted signal

     

    Synchronous detectors like this using square wave modulation work by assuming that the detector and input signal are perfectly in phase.

    What happens if the are not ?

     

    image

    I added a delay of 73uS, equivalent to 3.6degrees phase error to the input signal, the output has changed by about 4%.

    The point is not that this amount of variation in timing is likely or not but that this kind of detector is sensitive to edge timing.

    Square wave signals have worse problems than that - as we know a square wave is composed of s series of sinewaves, the fundamental

    and an infinite series of odd harmonics, amplitude decreasing with frequency. The 7th harmonic has an amplitude of 14.3% of the fundamental.

    Lets put a low pass filter on the input:

     

    image

    R6/C2 cuts the frequency response by 3dB at 1kHz and 6dB/octave thereafter.

     

    image

    And makes for an error of nearly 10% in the output.

     

    I need my sleep so there isn't time to model a phase sensitive detector tonight - I'll try tomorrow but I

    may have to use MATLAB because LTSpice isn't good at maths.

     

    SO you can run your own experiments here's the model:

     

    Version 4
    SHEET 1 1048 680
    WIRE 432 -48 256 -48
    WIRE 544 -48 512 -48
    WIRE 576 -48 544 -48
    WIRE 704 -48 656 -48
    WIRE 256 -16 256 -48
    WIRE 320 48 304 48
    WIRE 320 80 320 48
    WIRE 320 80 256 80
    WIRE 480 160 368 160
    WIRE 368 192 368 160
    WIRE 704 192 704 -48
    WIRE 80 208 48 208
    WIRE 256 208 256 80
    WIRE 256 208 160 208
    WIRE 336 208 256 208
    WIRE 544 224 544 -48
    WIRE 544 224 400 224
    WIRE 336 240 240 240
    WIRE -288 288 -384 288
    WIRE -80 288 -208 288
    WIRE 48 288 48 208
    WIRE 48 288 -80 288
    WIRE 80 288 48 288
    WIRE 240 288 240 240
    WIRE 240 288 160 288
    WIRE 368 288 368 256
    WIRE 480 288 480 160
    WIRE -384 320 -384 288
    WIRE 240 384 240 288
    WIRE -80 400 -80 288
    WIRE -384 448 -384 400
    WIRE 320 448 288 448
    WIRE 384 448 320 448
    WIRE 544 448 448 448
    WIRE 320 464 320 448
    WIRE 544 464 544 448
    WIRE -384 560 -384 528
    WIRE -80 560 -80 464
    WIRE -80 560 -384 560
    WIRE 240 560 240 480
    WIRE 240 560 -80 560
    WIRE 320 560 320 544
    WIRE 320 560 240 560
    WIRE 368 560 368 368
    WIRE 368 560 320 560
    WIRE 480 560 480 368
    WIRE 480 560 368 560
    WIRE 544 560 544 544
    WIRE 544 560 480 560
    WIRE 704 560 704 256
    WIRE 704 560 544 560
    WIRE 240 592 240 560
    FLAG 240 592 0
    FLAG 544 -48 UNF
    FLAG 704 -48 FIL
    FLAG 48 208 IN
    SYMBOL njf 304 -16 M0
    SYMATTR InstName J1
    SYMATTR Value 2N3819
    SYMBOL njf 288 384 M0
    SYMATTR InstName J2
    SYMATTR Value 2N3819
    SYMBOL OpAmps\\UniversalOpamp2 368 224 R0
    SYMATTR InstName U1
    SYMBOL res 176 192 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R1
    SYMATTR Value 100k
    SYMBOL res 176 272 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R2
    SYMATTR Value 200k
    SYMBOL res 528 -64 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R3
    SYMATTR Value 100k
    SYMBOL res 672 -64 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R4
    SYMATTR Value 10k
    SYMBOL cap 688 192 R0
    SYMATTR InstName C1
    SYMATTR Value 10µ
    SYMBOL res 304 448 R0
    SYMATTR InstName R5
    SYMATTR Value 100k
    SYMBOL diode 384 464 R270
    WINDOW 0 32 32 VTop 2
    WINDOW 3 0 32 VBottom 2
    SYMATTR InstName D1
    SYMATTR Value 1N4148
    SYMBOL voltage 368 272 R0
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V1
    SYMATTR Value -15
    SYMBOL voltage 480 272 R0
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V2
    SYMATTR Value 15
    SYMBOL voltage -384 432 R0
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V3
    SYMATTR Value SINE(0 1 50)
    SYMBOL voltage -384 304 R0
    WINDOW 3 -193 100 Left 2
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V4
    SYMATTR Value PULSE(-5 5 0 1u 1u .00365 .0073 500)
    SYMBOL voltage 544 448 R0
    WINDOW 3 -149 149 Left 2
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V5
    SYMATTR Value PULSE(10 -10 0 1u 1u .00365 .0073 500)
    SYMBOL res -192 272 R90
    WINDOW 0 0 56 VBottom 2
    WINDOW 3 32 56 VTop 2
    SYMATTR InstName R6
    SYMATTR Value 1
    SYMBOL cap -96 400 R0
    SYMATTR InstName C2
    SYMATTR Value 1.6e-4
    TEXT -184 -8 Left 2 !.tran 0 1 0

     

     

    Have fun.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to davemartin

    Hi Dave,

     

    I understand the need for assurance that the capability of older instruments and knowledge built on them is not lost.  Michael is doing a comparison of square wave with sinusoidal excitation.  And as Shabaz has pointed out the outlined design is quite capable of putting out a square wave and synching with it.  That should allow the value of a flexible design with additional capability to be assessed.

     

    Frank

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fmilburn
    fmilburn over 6 years ago in reply to davemartin

    Hi Dave,

     

    I understand the need for assurance that the capability of older instruments and knowledge built on them is not lost.  Michael is doing a comparison of square wave with sinusoidal excitation.  And as Shabaz has pointed out the outlined design is quite capable of putting out a square wave and synching with it.  That should allow the value of a flexible design with additional capability to be assessed.

     

    Frank

    • Cancel
    • Vote Up +3 Vote Down