• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56350 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
  • pdurdin
    pdurdin over 5 years ago in reply to michaelkellett

    That would be excellent. At the moment I'm limited to working with simulated readings, and it's just not the same!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • korrozivelab
    korrozivelab over 4 years ago in reply to michaelkellett

    Hi there!

     

    Wow! I'm very impressed about what you have achieved here in matter to create an ARP device. I'm not properly a geophysicist but I took some classes related with and since then, I've fallen in love with EM survey methods . Unfortunately I don't know about electronics or circuits so not much help i could bring you other than say you're awesome!. But what I think I can help with is giving some clues to address properly the problem of transmitter and receiver units, for example I've noticed (at least the few things of the thread I've read. It's too long!!) nobody has talked about electrode-ground contact as the main issue for transmitter or that the array device described by the OP is not the only one used to do a survey but it's the one that requires the largest S/N ratio, or something about telluric currents.

     

    Also I would like to help with field surveys, so, how much of development of the units have being achieved at this date? Is it possible to build something to test or i should go for the prototype mentioned by OP?

     

    Thanks to all of you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<