Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Nixie Tube Wristwatches
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 328 subscribers
  • Views 1166 views
  • Users 0 members are here
  • watch
  • hardware
  • diy
  • hobbyist
  • nixie
  • nixie_tube
Related

Nixie Tube Wristwatches

Catwell
Catwell over 15 years ago
I have seen Nixie Tube wristwatches for a while now.

image

Even Woz has one.

image

Now I want one too. Is there a place I can get one, as a kit perhaps? I found this site, but their kits are sold out : http://www.amug.org/~jthomas/watch.html
 
Does anyone ever worked with or have deep understanding of Nixie Tube control?

Cabe
  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Cabe - Nixie tubes are basically neon lamps and need around 90v across them to glow. Nowadays they call them Plasma TVs!

     

    There used to be a number of 74xx series chips which had high voltage capable (open collector effectively) outputs e.g. a BCD to decimal (1 of 10) decoder - one of those per tube and some counter chips and a handful of logic gates and you could make a timer - counter especially if you used (50Hz) FW rectified mains to get a 100Hz (10mS) tick. I suspect that the watch will have a PIC or similar running some counter code and a button that powers up an inverter when you want to read the time. I don't see why you shouldn't multiplex the displays although they never where originally. No doubt with all the development that went into plasma screens some bright spark has reinvented the wheel - with better efficiency and maybe lower operating voltages!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Bassman59
    Bassman59 over 15 years ago

    Woz's watch is made in Tucson by Cathode Corner. (http://cathodecorner.com/).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 15 years ago

    Cool - Thats "Almost" Steam Punk looking. If you could hide the battery and make the case Leather or wood, might just pass as Steam Punk. image