Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum 115V 400Hz Detect
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 326 subscribers
  • Views 459 views
  • Users 0 members are here
Related

115V 400Hz Detect

dmaruska
dmaruska over 15 years ago

I have a project that I need some help on.  I need to sence 115V AC 400Hz has been turned on/off.  I need that when the 115V is active on, it will light an LED (28vdc seperate supply).  The LED must stay on the entire time the 115V is present.  I have 3 Phases to monitor ( on or off).  Anyone have any ideas to do this?  I need to use and little power from the 115V as this is also monitored to see what the unit under test is utilizing (current <5ma).

 

Regards,

 

Dave M.

  • Sign in to reply
  • Cancel
Parents
  • R_Phoenix
    R_Phoenix over 15 years ago

    A simple solution would be a LED with about a 8K ohm 2watt resistor should do the trick. Connect it DIrectly to the 115v supply and ground if it's a common ground, or you can go between the Hot and neutral if you want.

    .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • R_Phoenix
    R_Phoenix over 15 years ago

    A simple solution would be a LED with about a 8K ohm 2watt resistor should do the trick. Connect it DIrectly to the 115v supply and ground if it's a common ground, or you can go between the Hot and neutral if you want.

    .