Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Need suggestions for a part
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 329 subscribers
  • Views 1289 views
  • Users 0 members are here
Related

Need suggestions for a part

R_Phoenix
R_Phoenix over 15 years ago

Hello all.

 

I am looking for the best option to detect when water is in a pipe. In a nut shell I 'm looking for a way to know when water is available inside a 3/4" pipe.

 

I thought of a pressure switch but I can't seem to find anything that is simple and in expensive and also there won't always be pressure on the switch, for instance when the water is flowing threw the pipe.

 

Then I thought of a flow meter, but again the water won't always be flowing to detect motion.

 

Now I am thinking of reading the capacitance/resistance of the water. I have a few options but I was wondering what else might be out there that I haven't stumbled on yet.

 

Thanks everyone.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    I had used a simple relative humidity sensor before by Honeywell.  The part was HIH-3610 that outputs a voltage level proportional to the supply voltage.  You might need to correct for environmental changes to humidity.  You would probably get a good  distinct reponse between the sensor element being wet or "dry" without having to do any corrections to the reading.

     

    Another idea, that might be a little tricky to implement would be some kind of "float" like you would find in a toilet, if there is water, a contact would float up and break contact with a switch, maybe a microswitch as was suggested earlier with something buoyant attached to a cantilever arm?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    I had used a simple relative humidity sensor before by Honeywell.  The part was HIH-3610 that outputs a voltage level proportional to the supply voltage.  You might need to correct for environmental changes to humidity.  You would probably get a good  distinct reponse between the sensor element being wet or "dry" without having to do any corrections to the reading.

     

    Another idea, that might be a little tricky to implement would be some kind of "float" like you would find in a toilet, if there is water, a contact would float up and break contact with a switch, maybe a microswitch as was suggested earlier with something buoyant attached to a cantilever arm?