Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Need suggestions for a part
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 329 subscribers
  • Views 1289 views
  • Users 0 members are here
Related

Need suggestions for a part

R_Phoenix
R_Phoenix over 15 years ago

Hello all.

 

I am looking for the best option to detect when water is in a pipe. In a nut shell I 'm looking for a way to know when water is available inside a 3/4" pipe.

 

I thought of a pressure switch but I can't seem to find anything that is simple and in expensive and also there won't always be pressure on the switch, for instance when the water is flowing threw the pipe.

 

Then I thought of a flow meter, but again the water won't always be flowing to detect motion.

 

Now I am thinking of reading the capacitance/resistance of the water. I have a few options but I was wondering what else might be out there that I haven't stumbled on yet.

 

Thanks everyone.

  • Sign in to reply
  • Cancel
Parents
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago

    Hi R,

     

    I think you're over thinking this. Since water conducts electricity, all you need is two conductors (non-corroding nails, or something that won't rust an contaminate the water supply). The two conductors form a switch, when no water is present the switch is open and no current flows. When water starts flowing in the pipe it will touch the two conductors and will allow current to flow from one to the other closing the switch.

     

    Two conductors and a pull-up resistor will give you a simple yes/no signal that you can feed to a microcontroller.

     

    hth,

    Jorge Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jvdberg@ieee.org
    jvdberg@ieee.org over 15 years ago in reply to Jorge_Garcia
    Pure water is an insulator. A small amount of contamination, like salt, will make water conducting. Depending of the water used in your system the conductivity test will not work.
    For heavily contaminated water a conducting path could remain when the pipe is dry.
    For a pressure sensor you could use the pressure sensors used to control the water level in a washing machine. The older ones have contacts that can handle several amps. These sensors are installed above the water level and filled with air. They measure the pressure at the bottom of the  reservoir. Remember that soap is very aggressive.
    Another way is to use the thermal conductivity of the water.
    Place a small NTC or PTC resistor, electrically insulated, in the pipe not touching the wall.
    Heat up this resistor with a small current. If there is water in the pipe the temperature of the resistor will be much lower than when the resistor is surrounded by air. Measuring the Voltage over the resistor will show weather there is water or not. If the temperature of the water could be high, place a reference circuit on the wall of the pipe and create a wheatstone bridge circuit.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jvdberg@ieee.org
    jvdberg@ieee.org over 15 years ago in reply to Jorge_Garcia
    Pure water is an insulator. A small amount of contamination, like salt, will make water conducting. Depending of the water used in your system the conductivity test will not work.
    For heavily contaminated water a conducting path could remain when the pipe is dry.
    For a pressure sensor you could use the pressure sensors used to control the water level in a washing machine. The older ones have contacts that can handle several amps. These sensors are installed above the water level and filled with air. They measure the pressure at the bottom of the  reservoir. Remember that soap is very aggressive.
    Another way is to use the thermal conductivity of the water.
    Place a small NTC or PTC resistor, electrically insulated, in the pipe not touching the wall.
    Heat up this resistor with a small current. If there is water in the pipe the temperature of the resistor will be much lower than when the resistor is surrounded by air. Measuring the Voltage over the resistor will show weather there is water or not. If the temperature of the water could be high, place a reference circuit on the wall of the pipe and create a wheatstone bridge circuit.