Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Need suggestions for a part
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 329 subscribers
  • Views 1289 views
  • Users 0 members are here
Related

Need suggestions for a part

R_Phoenix
R_Phoenix over 15 years ago

Hello all.

 

I am looking for the best option to detect when water is in a pipe. In a nut shell I 'm looking for a way to know when water is available inside a 3/4" pipe.

 

I thought of a pressure switch but I can't seem to find anything that is simple and in expensive and also there won't always be pressure on the switch, for instance when the water is flowing threw the pipe.

 

Then I thought of a flow meter, but again the water won't always be flowing to detect motion.

 

Now I am thinking of reading the capacitance/resistance of the water. I have a few options but I was wondering what else might be out there that I haven't stumbled on yet.

 

Thanks everyone.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello, There are several systems that could be employed 1) Conductivity, which is used in commercial water purification and typically indicates when the resistance is below 22 mohms, and unless specifically purified (DI, RO or distilled) all water will be below this value. 2) Thermal conductivity, measures how much power it takes to maintain a given temperature in an electrically heated probe. 3) Capacitance, which should give a large change in the absence of water. 4) IR, a simple infrared optoisolator should work as water is not very transparent to IR. 4) Density, measure the change in the frequency of a quartz crystal/ or sound conductivity between two piezoelectric elements, one driven and the other a sensor. 5) Refractive index of a bare fibre optic or again, just the change in the intensity of what light gets through to a photodiode. Conductivity and capacitance are widely used in industry. I'm guessing that these sensors can be inserted in the pipe, if not the thermal conductivity or density can be used external to the piping system. I can dig up circuits for these if interested

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello, There are several systems that could be employed 1) Conductivity, which is used in commercial water purification and typically indicates when the resistance is below 22 mohms, and unless specifically purified (DI, RO or distilled) all water will be below this value. 2) Thermal conductivity, measures how much power it takes to maintain a given temperature in an electrically heated probe. 3) Capacitance, which should give a large change in the absence of water. 4) IR, a simple infrared optoisolator should work as water is not very transparent to IR. 4) Density, measure the change in the frequency of a quartz crystal/ or sound conductivity between two piezoelectric elements, one driven and the other a sensor. 5) Refractive index of a bare fibre optic or again, just the change in the intensity of what light gets through to a photodiode. Conductivity and capacitance are widely used in industry. I'm guessing that these sensors can be inserted in the pipe, if not the thermal conductivity or density can be used external to the piping system. I can dig up circuits for these if interested