Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum What would be best for this application? beagleboard? raspberry pi?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 331 subscribers
  • Views 2131 views
  • Users 0 members are here
Related

What would be best for this application? beagleboard? raspberry pi?

e14 Contributor
e14 Contributor over 13 years ago

Im starting a project to create an underwater camera system what will monitor fish. The system will need to integrate a camera system, which can take pictures when a sound occurs in the water. Obviously this will include the use of a hydrophone to measure sound pressure and an accelerometer to measure particle velocity as well. I have been looking at some embedded processors and wonder if anyone would know if a beagleboard or raspberry pi would be suitable? I am also looking at TI's TMS320c5515 boards.

 

any ideas/comments would be appreciated

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • johnsocm
    johnsocm over 13 years ago +1
    This sounds like quite the project! I agree with John as well but I would personally use a BeagleBone or BeagleBoard. I have been playing with one and the python makes programming very easy. It is very…
Parents
  • COMPACT
    COMPACT over 13 years ago

    In addition to using a beaglebone I strongly suggest that you get a suitable camera that has a very fast lens. This is to ensure that your pictures do not have the fish end up as just coloured smudges on a murky backdrop. Depending upon the depth you may also need to provide suitable lighting. As for sensing the fish you will probably need a sonar just like those used for fish finders as this can measure range.

    Another question to ask is whether the electronics need to be at depth. Depending upon the application the electronics aside from the camera and sensor could be floating on the surface of the water and even be solar charged.

    If you want this hermetically sealed without any penetrations (i.e. holes) you could use the TI QI power solution to provide power and act as a messaging conduit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to COMPACT

    @ COMPACT :     Would you be able to recommend any suitable cameras which would be able to record straight to sd using the beaglebord? Regarding lighting the initial prototype will not need to go very deep, it will be tested in a 2m deep tank which will have sufficient lighting. As for sonar sensors, that it a great concept however for the initial prototype it will just be turned on manually before an underwater sound occurs (e.g piling ) - start to take video/pictures of the fish before the sound, once the sound starts record the particle velocity and sound pressure and use these measurments with the video/ images we can look at hows these sounds effect fish behaviour.

    id be most likely looking at the unit being placed on the seabed.

     

    @ Joe :     I will definetly be looking at the camera cape. Regarding the breadboard cape, I have access to normal breadboards to use within my project, im pretty sure ill be able to use these with the beagleboard to keep costs down?

     

    Thanks for the replies

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi people,

     

    I have now recieved the beaglebone and have sucessfully opened up the cloud9 IDE using windows. Now I have started to play around with the beaglebone, however I have become stuck, as in i am not sure how to progress with the project using this board. Firstly I have an Labtec webcam, what would be the simplest way to take pictures using the webcam and store them to sd?

     

    It seems alot of people are having problems in connecting a webcam to the beaglebone, which i didnt think would be so hard.

     

    thanks and i will cary on trying

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi people,

     

    I have now recieved the beaglebone and have sucessfully opened up the cloud9 IDE using windows. Now I have started to play around with the beaglebone, however I have become stuck, as in i am not sure how to progress with the project using this board. Firstly I have an Labtec webcam, what would be the simplest way to take pictures using the webcam and store them to sd?

     

    It seems alot of people are having problems in connecting a webcam to the beaglebone, which i didnt think would be so hard.

     

    thanks and i will cary on trying