Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Detailed Steps to Install USBIP on pcDuino
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 326 subscribers
  • Views 903 views
  • Users 0 members are here
  • openhardware
  • pcduino
Related

Detailed Steps to Install USBIP on pcDuino

alvin_jin
alvin_jin over 12 years ago

USB/IP Project aims to develop a general USB device sharing system over IP network. To share USB devices between computers with their full functionality, USB/IP encapsulates “USB I/O messages” into TCP/IP payloads and transmits them between computers.

In this post, we explain the steps need to take to install USBIP on a pcDuino.

Because the default kernel doesn’t support USBIP, we need to rebuild the kernel with USBIP enabled.  We have published many posts about how to compile and replace kernel on pcDuino.  We are going to repeat here to refresh the memory.

In the kernel build post,  we build pcDuino kernel on a X86 PC with cross-compilation. In this post, we are going to show something interesting by building kernel on pcDuino itself. Besides the time it takes to build, another issue is the storage space on pcDuino. There are two ways to get around: one is to use a large SD card, and the other one is to use NFS to make an external storage area to pcDuino.

Extra Space provided by SD card:

Let’s look at first option, ‘extra space provided by SD card’. We use a 16G SD card and boot from this SD card.

In this work, we need to login as root user:

 

1

 

 

$sudo su

 

First, we need to download source files of kernel:

For your convenience, we hosted the kernel source files for pcDuino also at amazon cloud. We are going to work at at directory “ /lib/modules/3.4.29+”.

 

1

 

2

3

4

 

$cd  /lib/modules/3.4.29+

 

root@ubuntu:/lib/modules/3.4.29+#wget https://s3.amazonaws.com/linksprite/pcduino/kernel/linux-sunxi.tar.bz2

root@ubuntu:/lib/modules/3.4.29+#wget https://s3.amazonaws.com/linksprite/pcduino/kernel/sun4i_defconfig

root@ubuntu:/lib/modules/3.4.29+#tar jxf linux-sunxi.tar.bz2

USBIP_pcduino_1

We create a directory named ‘build’ under “/lib/modules/3.4.29+”, and we copy ‘
sun4i_defconfig’ to the directory ‘build’, and rename as ‘.config’.

 

1

 

2

 

root@ubuntu:/lib/modules/3.4.29+#mkdir build

 

root@ubuntu:/lib/modules/3.4.29+#cp ../linux-sunxi/sun4i_defconfig ../build/.config

Before we build the kernel, we need to install some necessary packages:

 

1

 

 

root@ubuntu:/lib/modules/3.4.29+#sudo apt-get install  u-boot-tools libncurses5 libsysfs-dev

 

Now we need to configure the kernel:

 

1

 

 

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi#make menuconfig O=../build

 

The menu looks like the following:

USBIP_pcduino_2

We first enter into ‘General setup —>’ by moving the cursor  to that line and press ‘ENTER’:

USBIP_pcduino_3

As shown on the above figure, we locate the line “Initial RAM filesystem and RAM disk (initramfas/initrd) support, and press ‘ENTER’ to remove the asterisk ‘*’.

Return to the previous interface by navigate to ‘Exit’, and then locate the line begins with ‘Device Drivers’:
USBIP_pcduino_4
Press ‘ENTER’ , and locate the line ‘Staging drivers”, and press ‘SPACE’ to enable it:
USBIP_pcduino_5
Press ‘ENTER’, and a new interface shows up:
USBIP_pcduino_6
Press ‘M’ on ‘USB/IP support (EXPERIMENTAL)’, [M] on ‘VHCI hcd’,  and [M] on ‘Host driver’:
USBIP_pcduino_7

Press ‘Exit’ to exit, and save the new configuration:

USBIP_pcduino_8

Change into the ‘build’ directory, and build the kernel:

 

1

 

 

root@ubuntu:/lib/modules/3.4.29+/build#make

 

The above process will take about 4 hours. Please wait patiently.

 

1

 

2

3

 

root@ubuntu:/lib/modules/3.4.29+/build#make modules

 

root@ubuntu:/lib/modules/3.4.29+/build#make modules_install

root@ubuntu:/lib/modules/3.4.29+/build#make uImage

As we are build the kernel on SD card, we need to mount ‘/dev/mmcblk0p2′. Otherwise, if we boot from NAND, we use /dev/nanda’ instead.

 

1

 

2

3

 

root@ubuntu:/lib/modules/3.4.29+/build#mount  /dev/mmcblk0p2   /boot

 

root@ubuntu:/lib/modules/3.4.29+/build#cp arch/arm/boot/uImage   /boot   -f

root@ubuntu:/lib/modules/3.4.29+/build#reboot

Next, we manually load the USBIP driver.

 

1

 

2

3

4

 

root@ubuntu:/lib/modules/3.4.29+/build#modprobe  usbip-core

 

root@ubuntu:/lib/modules/3.4.29+/build#modprobe  usbip-host

root@ubuntu:/lib/modules/3.4.29+/build#modprobe  vhci-hcd

root@ubuntu:/lib/modules/3.4.29+/build#nano /etc/modules

We add the following content to file ‘modules’:

 

1

 

2

3

 

usbip-core

 

usbip-host

vhci-hcd

Next, we are going to configure and compile USBIP. We will need source files of kernel to configure and compile USBIP.

We navigate to the working directory:

 

1

 

2

3

4

5

 

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi/drivers/staging/usbip/userspace# ls

 

AUTHORS  Makefile     README      autom4te.cache  config.h     config.status  configure.ac  install-sh  ltmain.sh  stamp-h1

COPYING  Makefile.am  aclocal.m4  cleanup.sh      config.h.in  config.sub     depcomp       libsrc      missing

INSTALL  Makefile.in  autogen.sh  config.guess    config.log   configure      doc           libtool     src

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi/drivers/staging/usbip/userspace#

Run ‘autogen.sh’ first:

 

1

 

 

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi/drivers/staging/usbip/userspace# ./autogen.sh

 

This will generate a file named ‘configure’:

 

1

 

2

3

 

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi/drivers/staging/usbip/userspace#./configure

 

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi/drivers/staging/usbip/userspace#make

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi/drivers/staging/usbip/userspace#make install

After the installation, we need to install the dependency package:

 

1

 

 

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi/drivers/staging/usbip/userspace#sudo apt-get install hwdata

 

Now we can start the usbip process:

 

1

 

 

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi/drivers/staging/usbip/userspace#sudo usbipd -D

 

Next, we can check the USB devices attached on pcDuino:

 

01

 

02

03

04

05

06

07

08

09

10

11

12

13

14

 

Local USB devices

 

=================

- busid 2-1 (1bcf:05ca)

         2-1:1.0 -> usbhid

         2-1:1.1 -> usbhid

 

- busid 3-1 (1a40:0101)

         3-1:1.0 -> hub

 

- busid 3-1.1 (1058:0740)

         3-1.1:1.0 -> usb-storage

 

- busid 3-1.3 (148f:5370)

         3-1.3:1.0 -> unknown

On pcDuino, we have a WD USB drive attached to pcDuino’s USB host.

We are ready to bind the WD USB drive. The command is as following:

 

1

 

2

 

root@ubuntu:/lib/modules/3.4.29+/linux-sunxi/drivers/staging/usbip/userspace# sudo usbip bind -b 3-1.1

 

bind device on busid 3-1.1: complete

In the above command ’3-1.1′ is the USB device ID found in ‘usbip list -l’.

Until now, we are done with the part on pcDuino. Next, we move to work on a Windows PC that need to accepts the USB drive that is attached on pcDuino.

The USBIP driver for Windows can be downloaded from usbip.  The downloaded usbip can be unzipped to C:.
USBIP_windows_1
USBIP_windows_2
Point the driver path to the usbip directory.
USBIP_windows_3
We can see that the driver is installed correctly:
USBIP_windows_4

Download USBIPexe, and unzip to c:\usbip as we did with the driver.

 

1

 

 

C:\usbip\usbip -l 192.168.1.15

 

USBIP_windows_5

where 192.168.1.15 is the IP address of pcDuino.

Run

 

1

 

 

C:\usbip>usbip -a 192.168.1.15 3-1.1

 

where 3-1.1 is the USB ID on pcDuino.

After this command is executed, we will see ‘New USB device found’ on Windows PC.

USBIP_windows_6

We will see the Windows PC treats the WD USB drive as if it was attached to itself:

USBIP_5