Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Use Go lang to control GPIO on pcDuino
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 326 subscribers
  • Views 344 views
  • Users 0 members are here
  • lang
  • go
  • pcduino
Related

Use Go lang to control GPIO on pcDuino

alvin_jin
alvin_jin over 13 years ago

In this post, we show how to use Go lang to control GPIO on pcDuino.

If you have updated the image, sometimes, GPIO is not loaded by default. We need to use commands to load GPIO:

  1. $sudo modprobe gpio
  2. $sudo modprobe adc
  3. $sudo modprobe pwm

The main program is as follows:

  1. package main
  2. import (
  3. "fmt"
  4. "./gpio"
  5. "time"
  6. )
  7. func main() {
  8. g, err := gpio.NewGPIOLine(7,gpio.OUT)
  9. if err != nil {
  10. fmt.Printf("Error setting up GPIO %v: %v", 18, err)
  11. return
  12. }
  13.       blink(g, 100)
  14.       g.Close()
  15. }
  16. func blink(g *gpio.GPIOLine, n uint) {
  17. fmt.Printf("blinking %v time(s)\n", n)
  18. for i := uint(0); i < n; i++ {
  19. g.SetState(true)
  20. time.Sleep(time.Duration(1000) * time.Millisecond)
  21. g.SetState(false)
  22. time.Sleep(time.Duration(1000) * time.Millisecond)
  23. }
  24. }

The package used is shown below:

  1. package gpio
  2. import (
  3.      "fmt"
  4.      "os"
  5. )
  6. type GPIOLine struct {
  7.      Number uint
  8.      fd     *os.File
  9. }
  10. const (
  11.      IN = iota
  12.      OUT
  13. )
  14. func NewGPIOLine(number uint, direction int) (gpio *GPIOLine, err error) {
  15.      gpio = new(GPIOLine)
  16.      gpio.Number = number
  17.         err = gpio.SetDirection(direction)
  18.      gpio.fd, err = os.OpenFile(fmt.Sprintf("/sys/devices/virtual/misc/gpio/pin/gpio%d", gpio.Number), os.O_WRONLY|os.O_SYNC, 0666)
  19.      if err != nil {
  20.           return nil, err
  21.      }
  22.      return gpio, nil
  23. }
  24. func (gpio *GPIOLine) SetDirection(direction int) error {
  25.      df, err := os.OpenFile(fmt.Sprintf("/sys/devices/virtual/misc/gpio/mode/gpio%d", gpio.Number), os.O_WRONLY|os.O_SYNC, 0666)
  26.      if err != nil {
  27.           return err
  28.      }
  29.      fmt.Fprintln(df, "out")
  30.      df.Close()
  31.      return nil
  32. }
  33. func (gpio *GPIOLine) SetState(state bool) error {
  34.      v := "0"
  35.      if state {
  36.           v = "1"
  37.      }
  38.      _, err := fmt.Fprintln(gpio.fd, v)
  39.      return err
  40. }
  41. func (gpio *GPIOLine) Close() {
  42.      gpio.fd.Close()
  43. }

 

The code can be downloaded from pcduinogo.tar

Please download the above code to “$HOME/mygo”. To run the code, we do “$go run blink.go”.

IMG_2574

IMG_2572

IMG_2573