Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Kickstarter For Open Source GPU
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 328 subscribers
  • Views 3937 views
  • Users 0 members are here
  • oshw
  • fpga
  • gpu
Related

Kickstarter For Open Source GPU

morgaine
morgaine over 13 years ago

Well, this is a turn-up for the books:  a Kickstarter for "Open Source Graphics Processor (GPU)". !!!

 

There's a lot of "if's" involved, but it's certainly a very interesting idea, and worth exploring for multiple reasons, education and fun among others.

 

OSHW and FPGA enthusiasts having their own GPU would be fascinating! image

 

===

 

PS. I've been wondering whether the Parallella board wouldn't be a nice implementation platform for the programmable pipeline of a modern open-source GPU.  After all, the Epiphany device provides hardware parallelism with fast floating point for the core compute engines of 16 to 64 shaders without having to implement CPUs in Verilog.  The FPGA would then be left to do only the fastest parts of the overall task instead of implementing the programmable shaders that CPUs are best at.

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 13 years ago in reply to fustini +1
    And further on the topic of open source graphics: Today's report on Slashdot about "Open-Source Intel Mesa Driver Now Supports OpenGL 3.2" which has a few interesting explanatory posts in the comments…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine +1
    Morgaine Dinova wrote: Ah, but my view of OSHW and SW is fundamentally different to that market-centric one. I believe strongly that market penetration and success is completely irrelevant and even a hindrance…
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem +1
    John Beetem wrote: Guzunty Pi is wonderful because it uses the only CPLD I know of that's still available in a PLCC, which in turn has a pin grid array socket with 0.1" centers. Every other FPGA/CPLD that…
Parents
  • fustini
    fustini over 13 years ago

    Thanks for pointing this out!  I just backed it image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to fustini

    And further on the topic of open source graphics:

     

    • Today's report on Slashdot about "Open-Source Intel Mesa Driver Now Supports OpenGL 3.2" which  has a few interesting explanatory posts in the comments,
    • The same story but from the horse's mouth and with much more detail at Phoronix, "Mesa 10.0 Is Declared: OpenGL 3.2 Comes For Intel Linux".
    • An informative article by Phoronix from a week ago on the practical state of open source graphics on hardware accelerated cards, "16-Way Graphics Card Comparison On Open-Source Linux".

     

     

    It's been a difficult voyage for open source, but I think it's clear that the community is getting there even in the area that used to be the exclusive domain of closed graphics blobs from the card manufacturers.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago in reply to fustini

    And further on the topic of open source graphics:

     

    • Today's report on Slashdot about "Open-Source Intel Mesa Driver Now Supports OpenGL 3.2" which  has a few interesting explanatory posts in the comments,
    • The same story but from the horse's mouth and with much more detail at Phoronix, "Mesa 10.0 Is Declared: OpenGL 3.2 Comes For Intel Linux".
    • An informative article by Phoronix from a week ago on the practical state of open source graphics on hardware accelerated cards, "16-Way Graphics Card Comparison On Open-Source Linux".

     

     

    It's been a difficult voyage for open source, but I think it's clear that the community is getting there even in the area that used to be the exclusive domain of closed graphics blobs from the card manufacturers.