Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Who wants a core?  How about 8?  FREE Parallax Propeller board for review
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 329 subscribers
  • Views 1637 views
  • Users 0 members are here
  • parallax
  • open_source
  • oshw
  • embedded
  • propeller
  • micrcontroller
  • open_source_hardware
Related

Who wants a core?  How about 8?  FREE Parallax Propeller board for review

fustini
fustini over 12 years ago

I have a Parallax P8X32A Propeller QuickStart board that I've not gotten the chance to use yet:

The P8X32A QuickStart is a simple and accessible development platform for the P8X32A Propeller microcontroller.
The QuickStart is an evaluation board for the Propeller. As an open-source reference design the QuickStart board provides basic Propeller circuitry. Developers may use our PCB layout files as their own to speed their project towards completion. As a project board the QuickStart is fully expandable and provides unimpeded access to all I/O pins through an expansion header but includes some button inputs and LEDs to demonstrate programming. With USB power and a selection of QuickStart Project examples it's also the fastest way to get up and running.

imageimage


imageimage

I'm going to give this board for free to a lucky a Community member with the request that the winner please write a review (either in the blog here in this group or somewhere else on the web).  It doesn't have to be anything fancy - don't be intimidated.  Sorry, no minors, you must be 18 years of age or older!

 

To enter, do the following:

 

  • Reply to this post with a short description of why you are interested (1 to 2 sentences is fine)
  • I'll will pick a winner at random on Wednesday, November 13th, at 5pm US CDT.


Note: I'm located in Chicago and will ship it for free to the winner using the lowest cost option available.  If the winner is located outside the US, then the winner will be responsible for paying any customs fees or duty that may apply.  I will list the value as $35 USD.


I'll also include this robot badge, too:

image


Cheers,

Drew

http://twitter.com/pdp7

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago +1
    In addition to the Parallax boards being OSHW, the very nice P8X32A Propeller has 8 real physical cores on the chip, the real thing (they call them " cogs "), unlike the 8 so-called "logical cores" of…
Parents
  • morgaine
    morgaine over 12 years ago

    In addition to the Parallax boards being OSHW, the very nice P8X32A Propeller has 8 real physical cores on the chip, the real thing (they call them "cogs"), unlike the 8 so-called "logical cores" of the low-end XMOS SoCs which actually have only a single physical core whose throughput is partitioned into threads that have correspondingly reduced throughout.  (XMOS marketing has taken the liberty of renaming those threads "logical cores" recently, but it makes no engineering sense.)

     

    The 8 real physical cores of the Parallax SoC each contribute to the chip's overall throughout, as one would expect.  It's a lovely device with a huge amount of interfacing potential, so those wanting to enter the age of multicore microcontroller programming should take up Drew's excellent offer!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago

    In addition to the Parallax boards being OSHW, the very nice P8X32A Propeller has 8 real physical cores on the chip, the real thing (they call them "cogs"), unlike the 8 so-called "logical cores" of the low-end XMOS SoCs which actually have only a single physical core whose throughput is partitioned into threads that have correspondingly reduced throughout.  (XMOS marketing has taken the liberty of renaming those threads "logical cores" recently, but it makes no engineering sense.)

     

    The 8 real physical cores of the Parallax SoC each contribute to the chip's overall throughout, as one would expect.  It's a lovely device with a huge amount of interfacing potential, so those wanting to enter the age of multicore microcontroller programming should take up Drew's excellent offer!