Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum OpenBCI: connect your brain to your computer!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 326 subscribers
  • Views 3423 views
  • Users 0 members are here
  • kickstarter
  • open_source
  • eeg
  • bci
  • open_hardware
  • arduino
  • open_source_hardware
  • openbci
Related

OpenBCI: connect your brain to your computer!

fustini
fustini over 12 years ago

Here's an interesting Open Source Hardware kickstarter that I recently backed.  I thought others might find it interesting too:

image

 

OpenBCI: An Open Source Brain-Computer Interface For Makers

http://www.kickstarter.com/projects/openbci/openbci-an-open-source-brain-computer-interface-fo

OpenBCI is a low-cost, programmable, open-source EEG platform that gives anybody with a computer access to their brainwaves. Our vision is to realize the potential of the open-source movement to accelerate innovation in brain science through collaborative hardware and software development. Behind the many lines of code and circuit diagrams, OpenBCI has a growing community of scientists, engineers, designers, makers, and a whole bunch of other people who are interested in furthering our understanding of the brain

 

image

In the OpenBCI Brainwave Visualizer above, the graphic at the top left shows the electrode placement positions for the experiment. The color intensity of each node indicates the EEG wave amplitude at that region of the scalp [...] The screenshot was captured about 4 seconds after our test subject closed her eyes. There is a high amplitude waveform seen clearly in channels 5-8, which are placed on the back of the scalp. Notice a spike in the FFT graph at about 10-12Hz. This shows a predominance of alpha waves in the occipital region of the brain, which is what one would expect to see when the subject’s eyes are closed and the visual cortex has nothing to do

 

Anyone up for some brain hacking? image

 

cheers,

drew

http://twitter.com/pdp7

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago in reply to vsluiter +2
    Oh no - I'm going to have to be a PITA again. This is a nice project but it's abosulutely NOT SAFE !!! There is a reason that medical electronics has to pass much more stringent specs for safety than a…
  • morgaine
    morgaine over 12 years ago +1
    The subject area and the goals are interesting, but whoever thought up the "artistic" positioning of connectors in a semicircle deserves a severe whipping. Clearly someone thinks that it's an arts project…
  • shabaz
    shabaz over 12 years ago in reply to morgaine +1
    It's an interesting TI chip they're using. I just skim-read the kickstarter page, and couldn't tell the reason for the board shape, but I think maybe they expect to mount it inside a cap, rather than a…
Parents
  • morgaine
    morgaine over 12 years ago

    It should be pointed out that we seem to be discussing how to re-implement a very complex project which the Kickstarter would provide already working out of the box based on a chip designed for the purpose.

     

    If the end goal is to use rather than to design, the Kickstarter unit is likely to be a more effective approach. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago

    It should be pointed out that we seem to be discussing how to re-implement a very complex project which the Kickstarter would provide already working out of the box based on a chip designed for the purpose.

     

    If the end goal is to use rather than to design, the Kickstarter unit is likely to be a more effective approach. image

     

    Morgaine.