Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum MAKE: "Building an Open Source Laptop"
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 327 subscribers
  • Views 664 views
  • Users 0 members are here
  • maker
  • bunnie
  • open_source
  • oshw
  • make
  • diy
  • fpga
  • open_hardware
  • laptop
  • open_source_hardware
Related

MAKE: "Building an Open Source Laptop"

fustini
fustini over 12 years ago

The most excellent Bunnie has blogged on MAKE about his Open Source laptop project:

image

Building an Open Source Laptop | MAKE

About a year and a half ago, I engaged on an admittedly quixotic project to build my own laptop. By I, I mean we, namely Sean “xobs” Cross and me,bunnie  [...] Before this project, I had never designed with Gigabit Ethernet (RGMII), SATA, PCI-express, DDR3, gas gauges, eDP, or even a power converter capable of handling 35 watts [...] Building my own laptop would be a great way for me to stretch my legs a bit without the cost and schedule constraints normally associated with commercial projects.

 

The final bit of motivation is my passion for open hardware. I’m a big fan of opening up the blueprints for the hardware you run – if you can’t hack it, you don’t own it.

 

Here's the design files:

Novena Main Page - Studio Kousagi Wiki

 

and I'm sure it will excite some here that it also has a FPGA:

The machine must be useful as a hardware hacking platform. This drives the rather unique inclusion of an FPGA into the mainboard.

from the wiki page above:

Spartan-6 CSG324-packaged FPGA — has several interfaces to the CPU, including a 2Gbit/s (peak) RAM-like bus — for your bitcoin mining needs. Or whatever else you might want to toss in an FPGA.

It was also interesting to learn from Bunnie's blog post why he choose the Freescale i.MX6 quad core processor:

Freescale is the only SoC vendor in this performance class where you can simply go to their website, click a link, and download a mostly complete 6,000-page programming manual. It’s a ballsy move on their part and I commend them for the effort.


You can follow the project on Twitter: https://twitter.com/novenakosagi

 

cheers,

drew

http://twitter.com/pdp7

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 12 years ago +1
    Dr. Huang will be a keynote speaker at the EE Live! (formerly ESC) conference this April in San Jose, CA: Open Source Hardware and the Future of Embedded Systems Wednesday 2 April 9:30-10:30AM I'm looking…
  • fustini
    fustini over 12 years ago +1
    Another recent post on Make: Make Your Own Cellphone | MAKE "David Mellis* from the MIT Media Lab has been designing and refining his DIY cellphone , one that you can build yourself from his open source…
  • johnbeetem
    johnbeetem over 12 years ago

    Dr. Huang will be a keynote speaker at the EE Live! (formerly ESC) conference this April in San Jose, CA:

     

    Open Source Hardware and the Future of Embedded Systems

    Wednesday 2 April 9:30-10:30AM

     

    I'm looking forward to the talk.  Now, if he could just talk Xilinx into opening up that Spartan 6...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 12 years ago in reply to johnbeetem

    Darn it, now you have me wanting to go to EE Live image  I wish it was lined up closer to the Embedded Linux Conf (Embedded Linux Conference | Linux Conferences and Linux Events | The Linux Foundation).  Also in SJ but at the end of April.  I'm planning to take a vacation to attend it for the first time after jkridner told me I'd like it (my two fav things are Linux and embedded after all!).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 12 years ago

    Another recent post on Make:

     

    Make Your Own Cellphone | MAKE

    "David Mellis* from the MIT Media Lab has been designing and refining his DIY cellphone, one that you can build yourself from his open source design files and code. A “difficult, but potentially do-able project,” the phone has the basic features that you’d expect: you can make and receive calls and text messages and it has a phone book for storing numbers. To coincide with CES, we got an update from David on his homebrew consumer electronics device."

    *David Mellis is part of the Arduino team.