Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Novena: Open Source Hardware laptop launches!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 329 subscribers
  • Views 5240 views
  • Users 0 members are here
  • bunnie
  • open_source
  • imx6
  • xilinx
  • fpga
  • imx6quad
  • freescale_imx6
  • novena
  • open_hardware
  • laptop
  • arm
  • open_source_hardware
  • spartan
  • bunnie_huang
Related

Novena: Open Source Hardware laptop launches!

fustini
fustini over 12 years ago


image

Open Source Hardware laptop from Bunnie has launched!  Hackaday reports:

[Bunnie] Launches the Novena Open Laptop


Today [Bunnie] is announcing the launch of the Novena Open Laptop. When we first heard he was developing an open source laptop as a hobby project, we hoped we’d see the day where we could have our own. Starting today, you can help crowdfund the project by pre-ordering a Novena.


The Novena is based on the i.MX6Q ARM processor from Freescale, coupled to a Xilinx Spartan 6 FPGA. Combined with the open nature of the project, this creates a lot of possibilities for using the laptop as a hacking tool. It has dual ethernet, for routing or sniffing purposes. USB OTG support lets the laptop act as a USB device, for USB fuzzing and spoofing. There’s even a high speed expansion bus to interface with whatever peripheral you’d like to design.


The crowd funding campaign has kicked off on Crowd Supply:

Crowd Supply: Novena


A new open-hardware computing platform, flexible and powerful, designed for use as a desktop, laptop, or standalone board.

 

It looks like its off to a strong start.  Already at $57,715 raised of $250,000 goal with 45 days left.

 

Cheers,

Drew

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 11 years ago +3
    Thought I would follow up as my Novena laptop arrived in April. It's working great! Here's some photos: https://plus.google.com/photos/+DrewFustini/albums/6136930117627578369 Thanks to bonnie555 for helping…
  • johnbeetem
    johnbeetem over 10 years ago +3
    Bunnie Huang and Sean Cross have a nice write-up of Novena in the latest IEEE Spectrum : Novena: A Laptop With No Secrets - IEEE Spectrum They talk about the FPGA a lot, which is good, but they neglect…
  • fustini
    fustini over 10 years ago in reply to shabaz +3
    I think the Librem laptops from Purism will be closer to what an average consumer would want: https://puri.sm/ I've been following Purism with interest. Their blog has been very informative about the nitty…
Parents
  • johnbeetem
    johnbeetem over 10 years ago

    Bunnie Huang and Sean Cross have a nice write-up of Novena in the latest IEEE Spectrum: Novena: A Laptop With No Secrets - IEEE Spectrum

     

    They talk about the FPGA a lot, which is good, but they neglect to say that the FPGA is closed source like the GPU and you can't even run Xilinx tools on Novena itself.  I'm not criticizing Novena for selecting the Spartan-6, since it's a very nice part, but IMO an OSHW/SW project should be clear about what parts aren't open.  Also, they missed a fine opportunity to advocate for open FPGA bitstream documentation.

     

    Warning: while most of the comments at the IEEE Spectrum link are nice, some are pretty ugly.  Well, that's the Internet for you image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to johnbeetem

    john,

     

    I have read the article link you posted and Novena is not a new things, I started following this project by when Drew start noticing it. I remain skeptic... As a matter of fact, it sounds to me a circular concept; it is almost impossible - excluding to make the base CPU project from scratch - to have a open hardware device like a laptop with all parts full exposed, circuits schematics etc. They are appreciable because gone beyond the bare assembly another laptop, but most of the choices, especially the FPGA approach are something that needs a computer to manage this computer. But this sounds obvious to me. The point is that the price that this effort has generated IMO is too high respect the real benefits. As Shabaz says, it's a good dream, it's great to see it become reality but I see big difficulties that this product become popular and not a very specific niche jewel.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to johnbeetem

    john,

     

    I have read the article link you posted and Novena is not a new things, I started following this project by when Drew start noticing it. I remain skeptic... As a matter of fact, it sounds to me a circular concept; it is almost impossible - excluding to make the base CPU project from scratch - to have a open hardware device like a laptop with all parts full exposed, circuits schematics etc. They are appreciable because gone beyond the bare assembly another laptop, but most of the choices, especially the FPGA approach are something that needs a computer to manage this computer. But this sounds obvious to me. The point is that the price that this effort has generated IMO is too high respect the real benefits. As Shabaz says, it's a good dream, it's great to see it become reality but I see big difficulties that this product become popular and not a very specific niche jewel.

     

    Enrico