Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Making pcbs
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 329 subscribers
  • Views 4150 views
  • Users 0 members are here
  • raspberry
  • toner
  • hydrogen
  • pi
  • peroxide
  • chloride
  • copper
  • pcb
  • hydrochloric
  • acid
  • ferric
  • arduino
Related

Making pcbs

terrydark
terrydark over 12 years ago

Hi everyone,

 

This is my first discussion but I would like to see what the consensus is using  the knowledge and experience of all that have manufactured their own boards using "home brew" techniques.

 

In in your opinion, what is the best or perhaps economical and least fiddly of the methods for producing pcb boards via DIY?

 

Thanks in advance

 

Terry

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago +1
    As far as I know there is no convenient or free legal way of disposing of the waste products from etching copper from boards. In my youth (alas distant, early 1970s) I poured it down the drain but I understand…
  • D_Hersey
    D_Hersey over 12 years ago in reply to michaelkellett +1
    I have a set-up in my garage. Agitated ferric-chloride bath, tin plating, wet saw, ventilated drill press, xytable. I have a thermal press that directly transfers stencils from a laser-printer. Haven't…
  • johnbeetem
    johnbeetem over 12 years ago in reply to D_Hersey +1
    Don Hersey wrote: Another technique is to buy generic PCBs and modify them. The 'op-amp evaluation boards' from the few remaining linear players are better than I can make. Ebay ones from China for…
Parents
  • michaelkellett
    michaelkellett over 12 years ago

    As far as I know there is no convenient or free legal way of disposing of the waste products from etching copper from boards. In my youth (alas distant, early 1970s) I poured it down the drain but I understand that this is frowned upon now.

     

    Having said that, there are two methods which I have used, etching with Ferric Chloride solution and etching with a mixture of hydrochloric acid and hydrogen peroxide. Ferric Chloride needs to be agitated and works best if hot, hydrochloric acid and peroxide is quicker (and gets hot itself if too concentrated)  and cleaner. If you use photo resist you'll need sodium hydroxide solution to develop the resist, and some way of making photmasks. (Or you can paint the tracks on with paint or nail varnish (nail varnish is easy to remove)).

     

    There are now so many cheap sources of custom boards that I wouldn't bother to make my own - use stripboard or dead bug technique for quick lashups and bought in boards otherwise. PCBTrain and the like are perhaps too pricey for hobby stuff but there are several much cheaper sources if you don't mind waiting longer.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 12 years ago

    As far as I know there is no convenient or free legal way of disposing of the waste products from etching copper from boards. In my youth (alas distant, early 1970s) I poured it down the drain but I understand that this is frowned upon now.

     

    Having said that, there are two methods which I have used, etching with Ferric Chloride solution and etching with a mixture of hydrochloric acid and hydrogen peroxide. Ferric Chloride needs to be agitated and works best if hot, hydrochloric acid and peroxide is quicker (and gets hot itself if too concentrated)  and cleaner. If you use photo resist you'll need sodium hydroxide solution to develop the resist, and some way of making photmasks. (Or you can paint the tracks on with paint or nail varnish (nail varnish is easy to remove)).

     

    There are now so many cheap sources of custom boards that I wouldn't bother to make my own - use stripboard or dead bug technique for quick lashups and bought in boards otherwise. PCBTrain and the like are perhaps too pricey for hobby stuff but there are several much cheaper sources if you don't mind waiting longer.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • D_Hersey
    D_Hersey over 12 years ago in reply to michaelkellett

    I have a set-up in my garage. Agitated ferric-chloride bath, tin plating, wet saw, ventilated drill press, xytable.  I have a thermal press that directly transfers stencils from a laser-printer. Haven't used any of it in years.  Another technique is to buy generic PCBs and modify them.  The 'op-amp evaluation boards' from the few remaining linear players are better than I can make.  Ebay ones from China for that sell for pocket change are as good as I make them.

    Silicon connections are more reliable than PCB ones.  If it is digital and at all complex, I use a PROM if my I/O is balanced, otherwise programmable logic.  MCU evaluation boards have come along and are cheap.

     

    Short of it is that I agree with you and am only trying to re-enforce you, Michael, in this.  PCB milling plus hole collars is the way to go nowadays if one insists.  Fun thing to do/have done, though.  Zoning won't allow any solns with Cu in them down the drain, so it doesn't matter.  SMT tech has apaced the small player.

     

    Simulate.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to D_Hersey

    Don Hersey wrote:

     

    Another technique is to buy generic PCBs and modify them.  The 'op-amp evaluation boards' from the few remaining linear players are better than I can make.  Ebay ones from China for that sell for pocket change are as good as I make them.

    SchmartBoard and Adafruit (links included) have some very nice SMT adapter boards.  A few of those and some 0.1" grid perf board can make nice prototypes.  I still use wire-wrap on occasion.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 12 years ago in reply to johnbeetem

    I do as well.  Nowadays, I need magnifying glasses late at night, to look at it from the outside, it is really tedious, doing it can be a great flow experience.  My first W/W tools were of poor quality, which made things really frustrating.  When I got a coupla good WWguns and a nice stripper things got much nicer.  There seems to be some movement toward pins that have a metric basis.  Does anyone have experience with these?  Also, there seems to be a 2x scaled W/W scheme used on stereos from the seventies.  Any insights as to where these tools might be available?

     

    I have drawers full of surf boards.  If you are willing to wait for postage from the far sides of the globe, they can be very cheap.  So cheap that I inventory them rather than worry about the arrival of the mailman.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • terrydark
    terrydark over 12 years ago in reply to johnbeetem

    Thanks John, I actually have some of the adapter boards from Adafruit and they are great for development but I still need to design a pcb for testing before "production". I only plan 30 - 40 boards per run when I do them but I spent too much on revisions through the pcb manufacturers and my wife has said I have to find another way. I no longer have access to work facilities as I am retired.

     

    Regards

     

    Terry

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • terrydark
    terrydark over 12 years ago in reply to D_Hersey

    Yes, I just recently found my W/W tools and "had a go" but my eyes aren't what they used to be either and I quietly put the tools back in their box for prosperity or perhaps my son who may take an interest.

     

    Regards

     

    Terry