Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum The Switch and Transistor
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 328 subscribers
  • Views 801 views
  • Users 0 members are here
  • sp:on_semiconductor
  • pt:power
Related

The Switch and Transistor

e14 Contributor
e14 Contributor over 12 years ago

How the relay, switch, Vacuum tube and transistor brought us to the computer age.

The different between a mechanical switch and a transistor is that in a switch you can think of

it like a mechanical draw bridge that can interrupted or passes the flow off energy or water through it.

This switch require a mechanical movement to take place. Thus in a switch the amplification is your fingers or

muscle which open and close the flow of current. Note, the power of a switch can turn on one light in one room

or it can turn infinite lights in many other rooms on and off.

Here come the idea of the transistor with it's amplification, the amplification or electrical muscle can cause

one transistor to turn on or off many others transistor, like the mechanical switch except here the use of a movement is

not the finger but electrical signal to accomplish this. These lights or loads can store numbers, which intern can

represent,pictures,text,sound or any magnitude entity such as points on a screen.

Why a switch or transistor? Well these device can be also used as an on or off, true or false,

one and zero devices.Think about it, one in it self can be a multiple of any number(except zero). Just like you can

represent any decimal numbers in an infinite world with just ten symbol, therefore in a "binary system" with two symbol

you can also accomplish this task also, which they call machine language. So at the end, a simple device like a switch or

transistor can be very powerful instrument to be used.

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 12 years ago +1
    Well, any rational number anyway. It gives me the blues that you failed to mention an earlier device used for audio amplification, saturable reactor-based amps. Qs go back to 1928: Julius Edgar Lilienfeld…
Parents
  • D_Hersey
    D_Hersey over 12 years ago

    Well, any rational number anyway.  It gives me the blues that you failed to mention an earlier device used for audio amplification, saturable reactor-based amps.  Qs go back to 1928:  Julius Edgar Lilienfeld - Wikipedia, the free encyclopedia

     

    The idea of the generality of binary numbers is attributed to George Boole.  The idea that algorithms are generally serializable is attributed to Alan Turing.  A practical way to implement a Turing-equivalent machine is attributed John VonNeumann.

     

    We should not ignore man's long history of mechanical (and human) computing.  At the heart of computing is the analogy and the model.

     

    Brilliant analog computers have been created with boards, nails and soap bubbles.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to D_Hersey

    Thank you for the feedback. My explanation is in layman terms.

     

    Sent from my iPhone

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to D_Hersey

    Thank you for the feedback. My explanation is in layman terms.

     

    Sent from my iPhone