Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum 2 ethernet ports. is that posible?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 330 subscribers
  • Views 2611 views
  • Users 0 members are here
Related

2 ethernet ports. is that posible?

e14 Contributor
e14 Contributor over 10 years ago

Hi, we are in a tech project and we need a few raspberry pi 2B. But we need 2 ethernet ports. is that posible?

  • Sign in to reply
  • Cancel

Top Replies

  • gdstew
    gdstew over 10 years ago +1
    Yes, you can use USB to Ethernet (10/100 Mb/s) adapters which are readily available from lots of sources. You should check for compatibility (drivers) with the Raspberry Pi. If you need fairly high bandwidth…
Parents
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Another option using two ethernet is - without bridging and special differentiated usages - simply as a Round-robin management of the packets to optimise data transfer increasing the available network bandwidth. The point is that you have asked the question in terms of possibility; maybe good to know something more on the usage you plan with these two ethernet connections. As the Raspberry PI raspbian or jessie distributions are just Debian distro, you can also use the dual Raspberry PI ethernet to manage a different network segments routing, creating a - not so fast - reliable firewall and more.

     

    Is possible to have more details on what is the project use you plan?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Another option using two ethernet is - without bridging and special differentiated usages - simply as a Round-robin management of the packets to optimise data transfer increasing the available network bandwidth. The point is that you have asked the question in terms of possibility; maybe good to know something more on the usage you plan with these two ethernet connections. As the Raspberry PI raspbian or jessie distributions are just Debian distro, you can also use the dual Raspberry PI ethernet to manage a different network segments routing, creating a - not so fast - reliable firewall and more.

     

    Is possible to have more details on what is the project use you plan?

     

    Enrico