Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Sense Hat Detection?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 328 subscribers
  • Views 1913 views
  • Users 0 members are here
Related

Sense Hat Detection?

davidmoss1701@gmail.com
davidmoss1701@gmail.com over 10 years ago

I posted a question yesterday about a SenseHat error message that Python couldn't detect the device;

 

Python 3.4.2 (default, Oct 19 2014, 13:31:11)

[GCC 4.9.1] on linux

Type "copyright", "credits" or "license()" for more information.

>>> from sense_hat import SenseHat

>>> sense = SenseHat()

Traceback (most recent call last):

  File "<pyshell#1>", line 1, in <module>

    sense = SenseHat()

  File "/usr/lib/python3/dist-packages/sense_hat/sense_hat.py", line 36, in __init__

    raise OSError('Cannot detect %s device' % self.SENSE_HAT_FB_NAME)

OSError: Cannot detect RPi-Sense FB device

>>>

 

I have since done some research, and if I do a i2cdetect 1 command, I get in response 1c, 46,6a, 5c,and 5f!  Is this what I should see?  I am ready to return the device for another one if I can't sem to get this one to work, so any help would be greatly appreciated!

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Please anyone? I have the same problem....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Please anyone? I have the same problem....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Those are the correct i2c addresses for the sensors. 0x46 should have shown up as UU (that's the bus master)

     

    Have you tried to make sure all updates are installed?

     

    Have you tried this thread: https://www.reddit.com/r/raspberry_pi/comments/3yg0rz/sense_hat_and_jessie/

     

    There are many threads online about the Sense Hat. I've got an entire class of students using them successfully. I followed the directions at: https://www.raspberrypi.org/documentation/hardware/sense-hat/

    and created a micro SD image for the students. Worked first time, every time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer