Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum LiPo 3.3V Linear Regulation - Chip Suggestions?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 327 subscribers
  • Views 3833 views
  • Users 0 members are here
Related

LiPo 3.3V Linear Regulation - Chip Suggestions?

jgreenb8@gmail.com
jgreenb8@gmail.com over 10 years ago

Greetings,

 

I'm working with a design I developed and I'm running into the shortcomings of Inductor based regulators. I'm trying to regulate a 3.7V nom. lipo battery to 3.3V for ADC sampling of a strain gauge bridge. Unfortunately I am running into issues with noise and I believe it's due to the oscillations of the voltage regulator I am currently using, the TI TPS61200.

 

Does anyone know of a good linear voltage regulator that can take the 3.7-4.2 V of a LiPo and still hold a 3.3V stable output? 

 

I've searched for some time and I am not having much luck. Perhaps I am thinking of this from the wrong approach.

 

Many Thanks!

  • Sign in to reply
  • Cancel
  • jgreenb8@gmail.com
    0 jgreenb8@gmail.com over 10 years ago in reply to mlease

    I like the idea of decoupling the power system by using a separate regulator for the analog side and the digital side, this will most likely fix the problem. I'm not sure why I haven't considered that before, I just never thought to run two regulators on one circuit design.

     

    I think I've tried to put an RC filter before the MCU input before, not sure why it didn't make it to the PCB Design.

     

    Thanks a bunch for the help!

     

    Jacob G.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mlease
    0 mlease over 10 years ago in reply to jgreenb8@gmail.com

    Jacob, I hope that works for you. Using a 2nd regulator does make sense sometimes. If your WiFi isn't always connected it might make sense to put it on the switching regulator and have everything else running off an LDO. That way you could shut off the switching regulator when the WiFi isn't needed but then you have to worry about the state of signals between the micro and the WiFi module when the module is turned off so it probably isn't worth the trouble unless you have a tight power budget.

     

    The RC at the micro input would still be a good idea if the analog signal goes very far or is routed near the switching regulator.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<