Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum How is this RS485 module working?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 329 subscribers
  • Views 1529 views
  • Users 0 members are here
  • rs485
Related

How is this RS485 module working?

rishi2628
rishi2628 over 10 years ago

I am using an RS485 module :- http://www.elecrow.com/uart-ttl-to-rs485-twoway-converter-p-1545.html

This module is bidirectional and uses a single pair of differential signal to transmit/receive data. My question is how is the chip deciding whether it has to transmit data from TX to A+ B- or from A+ B- to RX?. Shouldn't there be 2 pairs of differential signal, one pair for TX and the other pair for RX? What is happening in this module??

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 10 years ago in reply to johnbeetem +2
    The clue is probably the diode in the middle. My guess would be a simple re-triggerable monostable (Schottky diode, cap and resistor) running from the transmit data to control the transceiver's direction…
  • johnbeetem
    johnbeetem over 10 years ago +1
    RS-485 is usually a half-duplex protocol with a single master and multiple slaves sharing a single A+B- differential pair. The master sends out a "poll" request and then disables its transmitter while…
  • gadget.iom
    gadget.iom over 10 years ago in reply to johnbeetem +1
    Hi johnbeetem I didn't want to add too much detail to yet another of these open-ended questions. But as this thread now has parties worth communicating properly with... I completely agree with your counterfeit…
Parents
  • johnbeetem
    0 johnbeetem over 10 years ago

    RS-485 is usually a half-duplex protocol with a single master and multiple slaves sharing a single A+B- differential pair.  The master sends out a "poll" request and then disables its transmitter while it waits for a reply.  The poll request includes an address, and the slave that matches the request replies to the poll, enabling its transmitter for the length of the message.  Only one device at a time drives the A+B- pair.

     

    I can't see how this module works.  Usually there's an extra TTL pin to enable the transmitter.  It's usually tied to the UART's RTS signal.  The product page does not show IC chip numbers, so you can't figure out how it works or whether the ICs are anything other than counterfeit junk.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to johnbeetem

    Hi johnbeetem

     

    I didn't want to add too much detail to yet another of these open-ended questions.

    But as this thread now has parties worth communicating properly with... image

     

    I completely agree with your counterfeit junk statement. They look like they contain an unbranded 485 transceiver and the other could be some sort of micro-controller. My impression is that this uC is buffering the UART and passing it to the transceiver while taking care of the data direction control.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to johnbeetem

    Hi johnbeetem

     

    I didn't want to add too much detail to yet another of these open-ended questions.

    But as this thread now has parties worth communicating properly with... image

     

    I completely agree with your counterfeit junk statement. They look like they contain an unbranded 485 transceiver and the other could be some sort of micro-controller. My impression is that this uC is buffering the UART and passing it to the transceiver while taking care of the data direction control.