Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum How to build a simple low cost reliable antenna switching circuit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 10 answers
  • Subscribers 327 subscribers
  • Views 9044 views
  • Users 0 members are here
  • ble 5.1
  • rf switch
  • timer circuit
Related

How to build a simple low cost reliable antenna switching circuit

BigG
BigG over 5 years ago

I'm looking to build a simple (MVP: minimal viable product) BLE antenna array circuit to test BLE direction finding (AoA/AoD) functionality.

 

I'm not wanting precision just yet. So, for my MVP I'm looking at just 3 maybe 4 antennas. For that I will need an RF switch and if I look on any of the major distributor websites I can find plenty single pole 3 or 4 throw (SP3T/SP4T) options.

 

My question is how to build the input control side, which usually consists of logic table like this one (for a SP4T RF switch):

 

Input 1Input 2
Output Mode
00RF1 on
01RF2 on
10RF3 on
11RF4 on

 

 

The switching frequency is at the microsecond(s) level.

 

My BLE chip is a single 3V3 MCU so I don't want to use this MCU to handle the switching as well as the other stuff. It's not a dual core PSoc, for example, where I could've used their hardware timer blocks etc.

 

So what IC options do I have with a power rail of 3V3.

 

Is it a case of using a precision Timer IC with some logic gates (e.g. OR, AND, NAND etc.) or would something like a tiny 8-bit MCU do the trick. Basically looking for as few components as possible which is low cost and reliable etc.

 

Looking to experts for some practical advice.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 5 years ago +8 suggested
    Hi Colin, By coincidence we're thinking on the same track : ) I've been looking at a silabs reference design, and aim to work as closely as possible to it, although it will take longer and is a pain due…
  • Fred27
    Fred27 over 5 years ago +7 suggested
    I recently needed to test out a NFC reader with multiple antennas. I grabbed a Peregrine Semi evaluation board (EK42441-03). It worked very well and it seems to fit your requirements, including the control…
  • BigG
    BigG over 5 years ago in reply to shabaz +5 suggested
    Just to add that when it costs less than $10, including postage, to get some prototype boards made I simply could not help myself... So I went ahead with a basic design. My limited understanding is that…
Parents
  • shabaz
    0 shabaz over 5 years ago

    Hi Colin,

     

    By coincidence we're thinking on the same track : )

    I've been looking at a silabs reference design, and aim to work as closely as possible to it, although it will take longer and is a pain due to the component sizes (smaller than I've ever fitted, so I might get it done for me).

    However, generally for RF switches, traditional popular choices are Peregrine Semiconductor and Skyworks, although there are options from others now too, e.g. NXP may have some. They are easy-ish to use, provided a few rules are followed. They mostly work with 3.3V logic. The inputs/outputs would need to be microstrip, that would be easiest, and there are online calculators for it. Some of the Peregrine parts are hand-solderable, and others may be too.

    For things like SP4T as you mention, one technique is to just use SPDT, and arrange one to feed two of them, i.e. a total of three SPDT can make a SP4T. The benefit being that sometimes it is easier to more symmetrically make the paths if you can spread them across separate chips, so that all paths are the same length (if that's what is desired depending on usecase).

    The chips can be controlled by normal logic gates, they are compatible with that, so a microcontroller to directly control them is fine too.

    Other than that, some basic RF prototyping rules can be followed, like complete ground plane, and any top side ground (generally just around the perimeter) must have lots of vias (spaced a couple of millimetres apart at a guess) to the underside ground. You might also want to consider 4-layer, in case it helps with the microstrip, since the width of that is determined by the distance to the groundplane, as you'll see with the calculators or use thinner PCB. Also, boards will warp, so with 2-layer you might want to consider having slightly more ground plane on top again with lots of vias, it's a balancing act. 4-layer and using the closest-to-top layer as ground plane is an option. Personally I'd go with 4-layer for this.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • BigG
    0 BigG over 5 years ago in reply to shabaz

    Hi Shabaz

     

    There's a saying "great minds think alike" but I think in my case it's just coincidence image

     

    Yes, the Silabs reference design is very handy alright.

     

    I've also come across a reference design from TI.

    http://software-dl.ti.com/simplelink/esd/simplelink_cc2640r2_sdk/2.30.00.28_new/exports/examples/rtos/CC2640R2_LAUNCHXL/…

    https://www.ti.com/lit/an/tida029/tida029.pdf

     

    And this project on Hackaday: https://hackaday.io/project/174175-micro-music

     

    My question is very basic and simply highlights my lack of electronics design know how and my uncanny knack of over complicating things.

     

    I'm simply wanting to evaluate or look at different hardware design options to offload the clock timer signal to trigger the RF switch logic as I have this notion that a micro second interrupt timer on my MCU will get in the way of doing other things.

     

    C://

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to BigG

    Hi Colin,

     

    As I understand (I could be wrong) the BLE stack on the chip is in control of the switching pins, so there's no need for any further consideration, apart from (perhaps) if you need to do any translation in logic to map to the signals required by the switches. If you're maybe aiming to do this yourself in your own code (wouldn't it need to be sync'd with the BLE chip tx or rx somehow? I don't know enough to be sure) then as far as microcontrollers go, as a ballpark, I think a 16MHz clocked processor would take about 1usec to get to a state from a timer interrupt where you have saved off enough registers and are ready to begin performing whatever you needed to do (of course, this is dependant on processor, RISC/CISC etc), so realistically you'd want at least a 48 MHz processor if not more. This is assuming you want to be using C and not assembler. I think I'd be wanting to process all three or 4 measurements within one timer interrupt when it occurs (and then you don't need as speedy a processor or as frequent timer interrupts). But this is still assuming that the BLE stack really cannot do it, so it's worth double-checking.

    Finally if you're just looking at repeatedly switching between antennas asynchronously that could be done with logic gates but I don't think this will work, so I guess I've misunderstood the requirement.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • BigG
    0 BigG over 5 years ago in reply to shabaz

    Thanks for the feedback Shabaz.

     

    Once again it pays to ask questions to the community... as I hadn't considered that may be the case... looking at the silabs docs again, the statement "The firmware for direction finding allows users to select antenna parameters such as the antenna array type" now makes sense. I hadn't put two & two together and considered the firmware aspect relating to antenna hardware design.

     

    I think I best read the documentation again.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • BigG
    0 BigG over 5 years ago in reply to shabaz

    Thanks for the feedback Shabaz.

     

    Once again it pays to ask questions to the community... as I hadn't considered that may be the case... looking at the silabs docs again, the statement "The firmware for direction finding allows users to select antenna parameters such as the antenna array type" now makes sense. I hadn't put two & two together and considered the firmware aspect relating to antenna hardware design.

     

    I think I best read the documentation again.

    • Cancel
    • Vote Up +4 Vote Down