Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Transformer winding
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 328 subscribers
  • Views 831 views
  • Users 0 members are here
Related

Transformer winding

ZeroSizeObject
ZeroSizeObject over 15 years ago
I want to wind my own transformer. What are some good techniques or references for such a task? I want to experiment with power transfer and winding ratios.
Zero
  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago
    The amount of power depends on the size and quality of the core.
    If you want to wind a transformer, first you must know the number of turns per Volt for the core you intend to use.
    If this is not known, you can determine this by winding a test coil. Slowly increase the AC-voltage on the test coil, until a fast rise in current is observed. Just below this point is the maximum voltage for this coil.
    With the number of turns per Volt known, you can calculate the number of turns for the voltages you need. Use 10% more secondary turns to compensate for the losses.
    With the total number of turns known, you can calculate the largest wire size that fits on the core you intend to use.
    For winding small transformers, with many turns of very thin wire, I can recommend a transformer winding machine. Big transformers are easier to  make without a transformer winding machine. What you need is a device to rotate the coil former. This device must have a brake to stop the process, for instance to insert an insulating layer.
    At http://webpages.charter.net/dawill/tmoranwms/Elec_Winding1.html you can see how simple this equipment could be.
    The winding equipment must also support the coil former to prevent it from bending under the pressure of the windings. Otherwise the core does not fit anymore.
    An electronic (or mechanical) turn counter is nice to have.
    Wind each turn next to the previous one and apply a layer of insulating paper after each layer of turns. Mechanical forces cause the windings to vibrate at the mains frequency if not properly fixed. Use glue, epoxi or high temperature tape to prevent this.
     
    For further reading see:
     
    http://en.wikibooks.org/wiki/Electronics/Transformer_Design
     
    http://en.wikipedia.org/wiki/Primary_winding
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago
    The amount of power depends on the size and quality of the core.
    If you want to wind a transformer, first you must know the number of turns per Volt for the core you intend to use.
    If this is not known, you can determine this by winding a test coil. Slowly increase the AC-voltage on the test coil, until a fast rise in current is observed. Just below this point is the maximum voltage for this coil.
    With the number of turns per Volt known, you can calculate the number of turns for the voltages you need. Use 10% more secondary turns to compensate for the losses.
    With the total number of turns known, you can calculate the largest wire size that fits on the core you intend to use.
    For winding small transformers, with many turns of very thin wire, I can recommend a transformer winding machine. Big transformers are easier to  make without a transformer winding machine. What you need is a device to rotate the coil former. This device must have a brake to stop the process, for instance to insert an insulating layer.
    At http://webpages.charter.net/dawill/tmoranwms/Elec_Winding1.html you can see how simple this equipment could be.
    The winding equipment must also support the coil former to prevent it from bending under the pressure of the windings. Otherwise the core does not fit anymore.
    An electronic (or mechanical) turn counter is nice to have.
    Wind each turn next to the previous one and apply a layer of insulating paper after each layer of turns. Mechanical forces cause the windings to vibrate at the mains frequency if not properly fixed. Use glue, epoxi or high temperature tape to prevent this.
     
    For further reading see:
     
    http://en.wikibooks.org/wiki/Electronics/Transformer_Design
     
    http://en.wikipedia.org/wiki/Primary_winding
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to jvdberg@ieee.org

    A really good post for someone who REALLY wants to make his own transformer. I found it also very interesting indeed.

     

    I would say to him that there are many more interesting areas of electronics than this, but each to his own!! I once made a transformer for an Oscilloscope that I built, once was enough!!

     

    I find that the huge offering of new & second-hand transformers in different sizes at a price I could not achieve as being very attractive…..plus the fact that Toroidal transformers are to my mind impossible for the private person to make and are far more  efficient than a standard transformer, take up less room, make less noise, make less heat, give out less electromagnetic waves and the sine wave is cleaner…..why would I even buy a normal transformer let alone make one?

     

    Regards

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago in reply to e14 Contributor
    Toroidal transformers with not too many turns could be made by hand. If you need a 115 Volt to low Voltage transformer, You could rewind the secondary of an existing transformer and use the existing primary winding.
    To wind a toroidal transformer by hand, you need a simple tool that fits trough the hole of the toroid. See drawing. First wind the wire on the tool. Then wind the transformer using this tool.image