Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Is there any inexpensive alternative similar to the rasberry , I could use for small media file server ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 328 subscribers
  • Views 900 views
  • Users 0 members are here
  • ftp
  • media
  • server
  • streaming
  • hd
Related

Is there any inexpensive alternative similar to the rasberry , I could use for small media file server ?

e14 Contributor
e14 Contributor over 14 years ago

I have tried several different options..using one of the  thinkpads.. i had lying around...  i tried a rack mount...  setup  with an epia micro-atx  board...   i even bougt a little used acer L100 figuring it would do the trick.... each project idea/ attempt,  ended in failure.       Ie,  the    L100 had    lan issues...     the thinkpad ..  obsolete   i486  system...... the   motherboard  build   the epia ,,  had no cd rom capacity.....

 

  I just cannot believe..  that a device such as a Playstation 3  is probably my cheapest option..  when  you consider the  hardware..  graphics..  and the software.?..   God forbid I try and compete graphically  with the PS3 ..LOL 

 

  I am at my last resolve...  i just purchased a really cheap blade server for $100   (ebay) and Windows Home Server 2011  for $50  newEgg ..  Figuring  this would be a bit of an overkill   but it would easily handle my desire for Streaming_media _Bliss !!

Once again  my efforts were a total failure....

 

Is there such a thing as a turn-key device that would network media ..  similar to the ps3 ?     yes I want it all  remote access  ...  HD.....  play-to......  nas  access......  ??? 

 

Am I asking to much?    I would love  access my security system also..  but I am having a hell of a time with the media portion !!!  

 

I would sincerely appreciate any input what so ever....    that any one could give....  On one last note..    My budget limits me to these doings....  thus..I would be willing to wait for a deal on EBAY.. for a particular....  shortcoming Vs....  just   outright purchasing a    $ XX,XXXX.00    device

 

Thank you in advance !

                                                                                                                     image

  • Sign in to reply
  • Cancel
Parents
  • fustini
    0 fustini over 14 years ago

    In terms of file server, there are compact Linux ones like SheevaPlug and GuruPlug:

     

    http://www.globalscaletechnologies.com/t-products.aspx

     

    CuBox is a compact Linux media player which is due out soon:

     

    http://www.solid-run.com/products/cubox

     

    For dedicated streaming media, I love my Roku:

     

    http://www.roku.com/roku-products

     

    And I've also hear good things about Boxee:

     

    http://www.boxee.tv/buy

     

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fustini
    0 fustini over 14 years ago

    In terms of file server, there are compact Linux ones like SheevaPlug and GuruPlug:

     

    http://www.globalscaletechnologies.com/t-products.aspx

     

    CuBox is a compact Linux media player which is due out soon:

     

    http://www.solid-run.com/products/cubox

     

    For dedicated streaming media, I love my Roku:

     

    http://www.roku.com/roku-products

     

    And I've also hear good things about Boxee:

     

    http://www.boxee.tv/buy

     

     

    Cheers,

    Drew