Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum i need a way to find a objects position and rotation?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 326 subscribers
  • Views 732 views
  • Users 0 members are here
  • hardware
  • diy
  • embedded
  • opensource
Related

i need a way to find a objects position and rotation?

e14 Contributor
e14 Contributor over 12 years ago

hi

i am a student looking for a way to find a objects x y and z and send this information to the pc

i have tried using an accelerometer but it can only tell me the rotation and i nedd to know how much the object is moving without using a caamera

thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • vsluiter
    0 vsluiter over 12 years ago

    An XYZ accelerometer will give you the orientation with respect to gravity when you're not moving. If you want to use an accelerometer to measure displacement, you'll have to integrate the acceleration twice, after removing the gravity vector (9.8g downward in world coordinates). The problem is that when you rotate fast, you'll also see acceleration, which is not caused by displacement. Also, you have to assume that the gravity vector will remain constant in direction during displacement.

    Integrating twice will also give a lot of offset over long term, so this would only work over short time frames.

     

    In 'professional' systems, the orientation is estimated by a combined accelerometer, gyroscope and magnetometer (generally Kalman filters are used here). Then, you at least know the direction of the gravity vector. When that is known, you could use the accelerometer for short term evaluation of displacement, and some other measured as described by Douglas or Mark for drift correction. But I guess that would be too much for a student assignment image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 12 years ago

    An XYZ accelerometer will give you the orientation with respect to gravity when you're not moving. If you want to use an accelerometer to measure displacement, you'll have to integrate the acceleration twice, after removing the gravity vector (9.8g downward in world coordinates). The problem is that when you rotate fast, you'll also see acceleration, which is not caused by displacement. Also, you have to assume that the gravity vector will remain constant in direction during displacement.

    Integrating twice will also give a lot of offset over long term, so this would only work over short time frames.

     

    In 'professional' systems, the orientation is estimated by a combined accelerometer, gyroscope and magnetometer (generally Kalman filters are used here). Then, you at least know the direction of the gravity vector. When that is known, you could use the accelerometer for short term evaluation of displacement, and some other measured as described by Douglas or Mark for drift correction. But I guess that would be too much for a student assignment image