Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Bus Pirate v5: A RP2040-based troubleshooting/programming tool has been released, and it looks interesting
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 28 replies
  • Subscribers 325 subscribers
  • Views 7663 views
  • Users 0 members are here
  • Bus Pirate
  • Bus Pirate v5
  • buspirate
  • rp2040
  • BusPirate v5
  • pi pico
Related

Bus Pirate v5: A RP2040-based troubleshooting/programming tool has been released, and it looks interesting

shabaz
shabaz over 2 years ago

I just saw this announced: a troubleshooting/development tool called Bus Pirate 5.

image (image source: buspirate.com)

The hardware and firmware source are on GitHub.

In a nutshell, the Bus Pirate 5 is a command-line controlled (via its serial console) tool that can be used to send/receive a few typical board-level (and other) protocols, such as SPI and I2C, and also UART (and some protocols on top). It would be nice to see additional protocols, but there is plenty of space for that - It runs with an RP2040 chip (a very straightforward part to code for!), with 16 Mbytes of Flash - but there's also an additional 100MBytes on a Flash chip for storing (say) firmware images to upload onto hardware. 

Interestingly, there is also a 1-5V supply on board with 500mA output capability, and this could be extremely handy.

What's also awesome is that the I/O (for eight pins) is configurable from 1.2V to 5V! That's extremely useful for the typical purposes of this board.

There is a plug-on LCD screen for monitoring purposes, plus (for reasons I don't understand yet, but perhaps it's handy for status and warning alerts, etc) there are also many RGB LEDs.

image(image source: buspirate.com)

The price is extremely reasonable (although the cables for it add to the cost - but they could be DIY'd).

I hope someone eventually writes a Python interface for this (otherwise, I will do it myself). I hoped to use the BeagleConnect Freedom (BCF) for similar purposes, but they are useless at getting information out for people to develop with it; mine has been a (small) dead brick for half a year. 

The Bus Pirate, on the other hand, is designed by Ian Lesnet. I purchased a couple of other boards originally designed by Ian (a logic analyzer and an FPGA board) a decade ago! They are excellent, so I've got high hopes for this board too.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +4
    Just kicking the tyre : ) I tried building it, that went smooth (except that on Ubuntu, I needed to type this first: sudo apt install libstdc++-arm-none-eabi-newlib After that, it was a normal build…
  • shabaz
    shabaz over 2 years ago +4
    I've not looked at it yet, but it arrived in a box the size of a paperback book. Inside were the two boxes for the BP5 and the optional probes.
  • shabaz
    shabaz over 2 years ago +4
    It comes _extremely_ well packaged! I want to know where Ian got these stickers made : ) Even comes with a hex/allen key to open it, and spares. In earlier photos I'd seen, the case looked like a 3D…
Parents
  • shabaz
    0 shabaz over 2 years ago

    A couple of bugs have crept into the PCB, so it is not shipping immediately. I received a very nice e-mail explaining the situation and stating that it will automatically be made right by shipping it resolved after CNY hols. However, the board issues are so minor, I think it's a shame to waste the PCB, so I've taken up the other option, to have it supplied with the issues, and I can self-fix.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • baldengineer
    0 baldengineer over 2 years ago in reply to shabaz

    Interesting... I did not receive the email, so I wonder if that means I was in batch 1 and it is already on its way?

    Tthanks for sharing the forum post!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to baldengineer

    Hi James, 

    Ah, in that case, we both will be self-fixing! : )

    I took a look at that MOSFET issue, and figured it could be resolvable in this way:

    The idea being to unsolder the tiny SOT-523 part and discard it, and then replace with a Si2301 in a more normal SOT-23 package, but rotated at 90 degrees anti-clockwise, and then two of the pins will fit. The last pin, Drain, would be connected with a wire link (shown in purple).

    It seems like this could be feasible anyway. I'll ask on the buspirate forum if I've made any error in the thinking here. The reason I chose the SOT-23 size part is because I have lots of those, and I don't have anything SOT-523. 

    image

    Another (slightly easier-to-follow) diagram of the same thing:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago in reply to baldengineer

    Hi James, 

    Ah, in that case, we both will be self-fixing! : )

    I took a look at that MOSFET issue, and figured it could be resolvable in this way:

    The idea being to unsolder the tiny SOT-523 part and discard it, and then replace with a Si2301 in a more normal SOT-23 package, but rotated at 90 degrees anti-clockwise, and then two of the pins will fit. The last pin, Drain, would be connected with a wire link (shown in purple).

    It seems like this could be feasible anyway. I'll ask on the buspirate forum if I've made any error in the thinking here. The reason I chose the SOT-23 size part is because I have lots of those, and I don't have anything SOT-523. 

    image

    Another (slightly easier-to-follow) diagram of the same thing:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 2 years ago in reply to shabaz

    Another option could be to get a SOT-523 MOSFET and flip it upside-down bend the legs down and solder it rotated partially, but that seems like it could be very awkward given the tiny size!