Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum The PAM8403 amplifier is very noisy
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 326 subscribers
  • Views 1850 views
  • Users 0 members are here
  • PAM8403
  • ws2812
Related

The PAM8403 amplifier is very noisy

me_Cris
me_Cris 5 months ago

Hi!

I was thinking of participating in a challenge but I ran into another challenge. Sweat smile
I'm using a small circuit with PAM8403 as a replacement for some speakers with dead audio circuit. In addition, I also have addressable LEDs in the case (this how they came) and I was thinking of using an MCU to control them. But I just noticed a very sharp and annoying noise produced when I power the LEDs, and it doesn't go away even when playing music.
I made a msall PCB, the schematic is below. The power supply is at 5V [USB]. I placed some capacitors in the idea to support the supply voltage.
What ideas do you have? What could I improve? 

Thanks!

The schematic:

image

The layout:

image

PAM8403 module:


image
The initial amplifier + controller board:

image
image

The speakers:
image

My assembly:

image

image


  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz 5 months ago +4
    Decided to quickly try that amp board, my results won't necessarily help at all since my setup is completely different and I don't have LEDs/microcontroller attached. I'm not near 'scope so I couldn't…
  • michaelkellett
    michaelkellett 5 months ago +3
    Do you have an oscilloscope. It will be much easier to fix the problem if you know what it is causing it. Since the noise happens when the LED is on it should be easy to see what is changing on the…
  • geralds
    geralds 5 months ago in reply to shabaz +2
    You're welcome. Oh, yes me too - I also have toys I can't remember why I have it. :) You mentioned the Vref _pin and -capacitor: It is important to know that this pin is a bi-directional pin. In…
  • shabaz
    shabaz 5 months ago in reply to geralds

    Hi Gerald,

    Thanks for the info, that part looks much better than the 8403. No reason to use that old part anymore. I can't recall the reason I had the 8403 board, I think I got it several years ago.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds 5 months ago in reply to shabaz

    You're welcome.

    Oh, yes me too - I also have toys I can't remember why I have it. :)

    You mentioned the Vref _pin and -capacitor:

    It is important to know that this pin is a bi-directional pin.

    In the datasheet is descripted you need a X7R cer. cap. between 470n to 1u.

    >>> Analog Reference Bypass Capacitor (CBYP)
    The Analog Reference Bypass Capacitor (CBYP) is the most critical capacitor and serves several important functions. During start-up or recovery from shutdown mode, CBYP determines the rate at which the amplifier starts up. The second function is to reduce noise caused by the power supply coupling into the output drive signal. This noise is from the internal analog reference to the amplifier, which appears as degraded PSRR and THD+N.
    A ceramic bypass capacitor (CBYP) with values of 0.47μF to 1.0μF is recommended for the best THD and noise performance. Increasing the bypass capacitor reduces clicking and popping noise from power on/off and entering and leaving shutdown.

    >>>

    But on the EMB is mounted a 100n X7R cap. This value is too small.

    This pin, Vref can modulate the signal through the signal path if that Vref value is not stabile. 
    Noise and popping noise signals are going to the amplifier.
    This cap. must be mounted very close to the pin and the GND must be a polygon field. - The polygon should be around the IC as well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • me_Cris
    me_Cris 5 months ago in reply to acdc90

    Hi, I'm a little late with the reply, I don't have much time during the week. Sweat smile
    I added pictures to the post.
    I'll experiment with the USB power supply part.
    I think LEDs (there are 7 per speaker) of this type consume enough mA (tens), and since I want to create some visual effects, I'm basically witnessing a "symphony" of noise.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • me_Cris
    me_Cris 5 months ago in reply to shabaz

    The PAM8403 module of this type is a little noisy (it's not for nothing that it costs very little), but it's clear to me that the LEDs produce a very sharp sound (I would describe it as a very annoying mosquito sound, I know it sounds strange what I'm saying Dizzy face).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • me_Cris
    me_Cris 5 months ago in reply to geralds

    Thank you, I will check that filter circuit.
    The PCB version is a bit homemade, so I can't make any claims.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • me_Cris
    me_Cris 5 months ago in reply to michaelkellett

    Not really, but maybe I don't need to go that far. I can also try other 5V powered circuits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • me_Cris
    me_Cris 5 months ago in reply to geralds

    I experimented a little by inserting a filter, I didn't use the same speakers (it's more difficult than it seems) but I noticed some reduction in "noise".
    Waiting for my PAM8406 version to arrive which should be improved on this side.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • me_Cris
    me_Cris 5 months ago in reply to shabaz

    I'm waiting for the PAM8406 version which should not be so noisy.
    I didn't achieve much using the ferrite bead + capacitors filter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • me_Cris
    me_Cris 5 months ago in reply to Gough Lui

    I did a test, I used the 5V power supply from the board to power another circuit also with addressable LEDs, and the noise is reduced (not by much) than when using LEDs that are already on the speaker. The noise source (addressable LEDs) being further away has some positive effect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds 5 months ago in reply to me_Cris

    Can you make photos of your assembled amp., that show us details about your built? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>