Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Practical Science Ideas for Primary School Kids
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 330 subscribers
  • Views 5108 views
  • Users 0 members are here
  • education help
  • stem education
  • practical_experiments
  • science_lessons
Related

Practical Science Ideas for Primary School Kids

shabaz
shabaz over 9 years ago

Hi,

 

I thought I'd ask on the community, long story short, I have a family member in another country who is a primary school teacher. Resources are tight, and she's looking for the best way to teach children science. She was thinking of Youtube videos, but I'm thinking practical experiments using easy-to-find objects like batteries, wires, thermometer, multi-meter, calculator, ruler, magnets, LEDs, bicycle pumps and coca-cola bottles, etc.

 

I noticed there are very few Kindle books on the topic, and the few seem just "average" from the previews. It actually seems a major shortcoming. There are plenty of schools in less fortunate parts of the world, and science experiments would really get kids excited I think.

 

If it doesn't already exist, I'm thinking of preparing a 'primary school lab' list of simple experiments and the items that could be useful, or a URL to more information. I can think of dozens of experiments (perhaps a hundred experiments) but surely there are good resources with this already. I'd rather just point her to a book or website if resources like this already exist.

 

Cost is an issue, so no experiments needing (say) large heavy microscopes, but a magnifier lens is ok. No bunsen burner connected to a supply, but a candle or ethanol burner is fine, and so on.

What are some good websites, or books, for such experiments? For sub-10-year-olds.

What resources do you use for teaching kids? If youtube videos, which ones?

 

Is it worthwhile maintaining such a list? If so, perhaps we can do so in the comments below, as an in-progress list.

Here are some examples for such a list:

 

electromagnet - wire, battery

radio transmitter - wire, battery, AM radio as receiver

flashing fire engine light - wire, battery, lamp, foil, toy fire engine

compass - pins, magnet

mini xmas tree lights - bag of LEDs, some resistors and a (say) 12V battery

intercom communication - two speakers and twin wire

electrostatics - balloons

generator - toy motor and lamp

 

Many thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +3
    Hi Shabaz, Experiment 1 Requires an ice cube, a string, and some salt. Question to the children: How can you pick up the ice cube without touching it using just the string and the salt? Answer: Place the…
  • shabaz
    shabaz over 9 years ago +3
    Hi ntewinkel jw0752 djfraz gecoz beacon_dave @DAB thanks so much for this detailed information. I'm sure all this will help her devise some great lessons in her school - the ideas here are so fantastic…
  • ntewinkel
    ntewinkel over 9 years ago +2
    That sounds like a great idea, Shabaz! I wonder if a wikipedia type setup would work well for that? Or maybe working with an existing platform like Instructables or Hackster. Then it just comes down to…
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi Shabaz,

     

    Experiment 1

    Requires an ice cube, a string, and some salt.

    Question to the children: How can you pick up the ice cube without touching it using just the string and the salt?

    Answer: Place the string on top of the ice cube and sprinkle some salt on it. The salt melts some of the ice as the temperature of freezing the salt water drops. This is an endothermic phase change so some of the non-salty water refreezes and this hopefully freezes the string to the ice and allows it to be picked up off the table.

    The science discussion can include heat as a form of energy. Phase change of water from solid to liquid to gas. The effect of how things like salt can change the freezing point. Even how they used to make ice cream before commercial refrigeration was available.

     

    Experiment 2

    Requires 2 marbles and a child with a good ability to shoot them. A small ramp that the teacher can aim is perhaps a better choice than my first suggestion.

     

    Variation one:

    Discuss elastic collisions and get the children to predict what will happen when the marbles collide at different angles.

     

    Variation two:

    Place one marble on the edge of the table and shoot the other marble at it so that one falls nearly straight down and the other continues off the table ballisticly. Get the children to predict which one will hit the floor first. Discuss how objects fall and the greater effect of air resistance on some objects which lead to the incorrect belief that heavier object fall faster.

     

    (Marbles are great for demonstrating all types of things)

     

    Experiment 3

    Requires small paper circle, a pencil, 3 crayons ( Red, Blue, Yellow), and some tape or glue.

     

    Draw alternating bands of color on the disk until you have a complete wheel of Red - Blue - Yellow repeated around it. Attach the disk to the pencil with glue or tape so that you can roll the pencil between your hands and thus spin the disk. You should be able to make the disk appear fairly white by doing this as a mixture of those colors reflected into our eyes is interpreted as White. By using just 2 of the colors in different proportions you can produce many other colors in this fashion too.

     

    Discussion about color and our perception of it.

     

    I bet the other guys on the forum can come up with tons of these that your family member can use that do not require anything but simple props.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 9 years ago

    Hi Shabaz,

     

    Experiment 1

    Requires an ice cube, a string, and some salt.

    Question to the children: How can you pick up the ice cube without touching it using just the string and the salt?

    Answer: Place the string on top of the ice cube and sprinkle some salt on it. The salt melts some of the ice as the temperature of freezing the salt water drops. This is an endothermic phase change so some of the non-salty water refreezes and this hopefully freezes the string to the ice and allows it to be picked up off the table.

    The science discussion can include heat as a form of energy. Phase change of water from solid to liquid to gas. The effect of how things like salt can change the freezing point. Even how they used to make ice cream before commercial refrigeration was available.

     

    Experiment 2

    Requires 2 marbles and a child with a good ability to shoot them. A small ramp that the teacher can aim is perhaps a better choice than my first suggestion.

     

    Variation one:

    Discuss elastic collisions and get the children to predict what will happen when the marbles collide at different angles.

     

    Variation two:

    Place one marble on the edge of the table and shoot the other marble at it so that one falls nearly straight down and the other continues off the table ballisticly. Get the children to predict which one will hit the floor first. Discuss how objects fall and the greater effect of air resistance on some objects which lead to the incorrect belief that heavier object fall faster.

     

    (Marbles are great for demonstrating all types of things)

     

    Experiment 3

    Requires small paper circle, a pencil, 3 crayons ( Red, Blue, Yellow), and some tape or glue.

     

    Draw alternating bands of color on the disk until you have a complete wheel of Red - Blue - Yellow repeated around it. Attach the disk to the pencil with glue or tape so that you can roll the pencil between your hands and thus spin the disk. You should be able to make the disk appear fairly white by doing this as a mixture of those colors reflected into our eyes is interpreted as White. By using just 2 of the colors in different proportions you can produce many other colors in this fashion too.

     

    Discussion about color and our perception of it.

     

    I bet the other guys on the forum can come up with tons of these that your family member can use that do not require anything but simple props.

     

    John

    • Cancel
    • Vote Up +3 Vote Down