Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Polls Open Source Hardware Success Factors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jeff
  • Date Created: 26 Oct 2010 3:30 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 1505 views
  • Likes 2 likes
  • Comments 5 comments
Related
Recommended

Open Source Hardware Success Factors

Which of the following factors are most critical to expanding the open source hardware movement? (log on to cast your vote!)

  • hackerspace
  • maker
  • amicus18
  • makerfaire
  • hardware
  • open
  • embedded
  • hobbyist
  • Design
  • source
  • arduino
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 16 years ago +2
    Extremely wel placed question! Since I am in Open Source Hardware I allways wonder why the industry accepts Open Source Software – even contributes – but has so much problems with Open Source Hardware…
  • Jeff
    Jeff over 16 years ago in reply to e14 Contributor +2
    I use to work for a semicondutor company and I always though it amusing that we would invest significant sums of money to create "development" platforms that were sold at a loss and had no hope of recouping…
  • Zad
    Zad over 16 years ago in reply to e14 Contributor +1
    To be honest, I see it as a new name for something that has been around since year 1. Much of what we as design engineers do is direct from the application notes, data sheets, or in some way "borrowed…
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    You only have to look at the success of initiatives such as the TI BeagleBoard which is low cost, open and has a cult following.  The key to success is that it is fully open source hardware which has enabled a much wider audience to get access to this technology fostering a cult following.  A number of BeagleBoard clones have been released based on the original design files which maybe add a few features or make it available in geographic regions not well served by the distribution network.  Big companies use these low-cost platforms alongside officially supported SV reference boards - reference board for getting official support,  open hardware boards for internal design innovation and prototypes.  They are also expendable! You can buy 10 BeagleBoards for the price of 1 OMAP3530 EVM for example!

     

    The latest generation of devices from all major SoC manufacturers are so complex that bare metal programming is just not an option any more hence the need to provide software OS support in order to make them do anything useful.  It is clear that open source / community priced software and hardware must be very tightly coupled with good support for any new hardware to be adopted.

     

    Good communications and visibility in the right places helps get the community engaged.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 16 years ago

    You only have to look at the success of initiatives such as the TI BeagleBoard which is low cost, open and has a cult following.  The key to success is that it is fully open source hardware which has enabled a much wider audience to get access to this technology fostering a cult following.  A number of BeagleBoard clones have been released based on the original design files which maybe add a few features or make it available in geographic regions not well served by the distribution network.  Big companies use these low-cost platforms alongside officially supported SV reference boards - reference board for getting official support,  open hardware boards for internal design innovation and prototypes.  They are also expendable! You can buy 10 BeagleBoards for the price of 1 OMAP3530 EVM for example!

     

    The latest generation of devices from all major SoC manufacturers are so complex that bare metal programming is just not an option any more hence the need to provide software OS support in order to make them do anything useful.  It is clear that open source / community priced software and hardware must be very tightly coupled with good support for any new hardware to be adopted.

     

    Good communications and visibility in the right places helps get the community engaged.