• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Polls Are any SBCs ready to replace desktop computers?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 16 Nov 2014 11:51 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:01 PM
  • Views 5857 views
  • Likes 1 like
  • Comments 27 comments
Related
Recommended

Are any SBCs ready to replace desktop computers?

I would love to replace my power-hungry desktop PC with an inexpensive SBC with no audible fan.  However, so far the SBCs I've tried lately (BeagleBone, Raspberry Pi, BeagleBoard) don't have enough processing power to be a viable desktop PC.

 

So, are any of the higher-performance SBCs that have been released lately up to the task?  I'm looking for a GNU/Linux computer that can do a decent job surfing the Internet (I don't care about video or audio performance) and a decent job compiling C programs.  I would say it needs at least 1 GB RAM and SATA for a disk drive.  100 Mb/s Ethernet is adequate, but I'd prefer not going through a USB hub.  Reasonable number of USB ports and HDMI output.  Wi-Fi is not needed or desired.

 

Here are some of the SBCs I've been watching and might consider.  Feel free to add others!  Most of these are OSHW, which is of course preferred.

 

Banana Pi: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

CubieTruck: Allwinner A20 Dual ARM Cortex-A7, 2 GB DDR3, SATA, GBE.

Intel Next Unit of Computing (NUC): Intel Atom or other, up to 8 GB DDR3, SATA, GBE.

MinnowBoard MAX: Intel Atom, 1 or 2 GB DDR3, SATA, GBE.

Olimex LIME2: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

PCduino3Nano: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

RIoTboard: Freescale i.MX6 ARM Cortex-A9, 1GB DDR3, no SATA, GBE.

Wandboard Quad: Freescale i.MX6 Quad ARM Cortex-A9, 2 GB DDR3, SATA, GBE.

  • sbc
  • oshw
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago +5
    Hi John! I've not used many of these, so I can't comment with much knowledge, but I suspect RIoTboard is getting there, certainly running Android it is speedy (if one is happy running Android to do work…
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild +3
    A nice pic of my XU on the back of one of my monitors.
  • fustini
    fustini over 11 years ago in reply to fustini +3
    johnbeetem - I've been using the MinnowBoard MAX as my 3-D printing workstation and love it! I have a USB 3.0 memory stick for the main disk running Ubuntu. It is really the first time I've used a single…
Parents
  • shabaz
    shabaz over 11 years ago

    Hi John!

     

    I've not used many of these, so I can't comment with much knowledge, but I suspect RIoTboard is getting there, certainly running Android it is speedy (if one is happy running Android to do work - I saw some recent post on theregister.co.uk where someone tried to run their business exclusively from a mobile phone all week - turns out they were quite successful!). I've not tried Linux on it.

    The Odroid-U3 is almost definitely a near-laptop replacement, I got very good performance running a desktop with Linux, and compiles were fast too. However it does have a heatsink! But no fan.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 11 years ago

    Hi John!

     

    I've not used many of these, so I can't comment with much knowledge, but I suspect RIoTboard is getting there, certainly running Android it is speedy (if one is happy running Android to do work - I saw some recent post on theregister.co.uk where someone tried to run their business exclusively from a mobile phone all week - turns out they were quite successful!). I've not tried Linux on it.

    The Odroid-U3 is almost definitely a near-laptop replacement, I got very good performance running a desktop with Linux, and compiles were fast too. However it does have a heatsink! But no fan.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    yes Shabaz I have some of those available too! image

     

    Not fast enough then you can get the XU or XU3 thunderbolts and lightning image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild

    A nice pic of my XU on the back of one of my monitors.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild

    And a video of the U3 which is the affordable quadcore...nice

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to Problemchild

    John Alexander wrote:

     

    A nice pic of my XU on the back of one of my monitors...

    I saw an XU3 at the ARM TechCon last October.  Very impressive hardware, with quiet little CPU fan that only turns on as needed.  There's now an XU3 Lite for $99 plus international shipping (or $105 in the USA) that sure looks like it could meet my desktop computing requirements.

     

    How is the ODROID community?  Have you been able to get answers as needed?  If I were to get an XU3 Lite I'd want to hook up an external USB 3.0 hard drive as my main file system.  Would you know if this is easy to do?  What a saw at http://forum.odroid.com/ was pretty confusing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to johnbeetem

    @John Beetem ,

         I would say probably should be fine. I have hooked up my Raspberry Pi to external USB 2.0 drives on a hub running OPENLEC for movies and the software perform great. image

     

    Clem