Passive Components
  • Technologies
  • More
Passive Components
Forum Hi there. I'm scratch building a large RC warship with lots of working features. I need a varisistor for speed control.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 110 subscribers
  • Views 1011 views
  • Users 0 members are here
Related

Hi there. I'm scratch building a large RC warship with lots of working features. I need a varisistor for speed control.

e14 Contributor
e14 Contributor over 11 years ago

I will be using 2 6vdc 7ah batteries which will give me 6vdc @ 14 ah and -with diodes- 12vdc @ 7 ah. The screws will be turned using 4  perm magnet motors. Thus i need to get a good versistor or whatever for additional speed control. what would you suggest?


Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • e14candies
    e14candies over 11 years ago +1
    I think you mean using or-ing diodes, you can run the batts in parallel (6V 14aH). In series (6+6=12V), no diode is needed. In any case, if you want to only go fwd, a PWM low side fet (meaning switching…
  • element14jamie
    element14jamie over 11 years ago +1
    Hello francist44 Welcome to the element14 Community, I will move this to the Passive area as it is a better fit. Thank you, Jamie
  • e14candies
    e14candies over 11 years ago

    I think you mean using or-ing diodes, you can run the batts in parallel (6V

    14aH).  In series (6+6=12V), no diode is needed.

     

    In any case, if you want to only go fwd, a PWM low side fet (meaning

    switching the gnd) is the easy way to go.  You could even use a 555 timer

    to set the percent on time (probably from 50% to max).  Other pulse

    circuits could give you a wider speed adjustment.

     

    If you need to go fwd &rev, then you need a full bridge (H-bridge), which

    is generally 4 fets (2 high side & 2 low side).  There are some chips that

    contain everything you need in one package(such as used for car electric

    windows).

     

    Always use care when playing with warships

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago

    Hi Frank,

    This sounds like a great project. Perhaps element14jamie will move your question on Monday to an area where it will get more replies.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • element14jamie
    element14jamie over 11 years ago

    Hello francist44

    Welcome to the element14 Community, I will move this to the Passive area as it is a better fit.

     

    Thank you,

     

    Jamie