Passive Components
  • Technologies
  • More
Passive Components
Forum Unusual Variable Inductor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 111 subscribers
  • Views 3927 views
  • Users 0 members are here
  • variable_inductor
Related

Unusual Variable Inductor

jw0752
jw0752 over 11 years ago

I was digging through my electronics graveyard and I found this interesting variable inductor. It has a ceramic drum wound with 14 gauge silver alloy wire. I measure a minimum to max range of 1uH to 12uH. As the drum is turned a small idler wheel rolls over the coil as a variable tap changing the amount of the coil that is included in the circuit. I was hoping that someone could tell me more about its original application. The square plates on the frame are 6.2 cm on a side and the length of the body is 9.5 cm. The front main shaft is coupled to the drum with an insulated universal joint. I see a shadow on the ceramic where there was likely a label at one time but it is gone now. If I can get a little more information about it I will put a tag on it so the next time someone runs across it there will not be a mystery.

 

image

 

image

 

image

 

image

 

Thanks John

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +2 verified
    To me, it looks like a medium-power 'roller inductor.' The gear makes me think it was intended to be operated by a motor. The most likely application was to tune an HF antenna. Yup, HF autotuner is my…
  • D_Hersey
    D_Hersey over 11 years ago +2
    I think due to its scale that this was used on the transmit side to normalize the load. The application circuit would have been along these lines: Pi-Match | Electronics and Electrical Engineering Tools…
  • jw0752
    jw0752 over 11 years ago in reply to shabaz +1
    Hi Shabaz, I was thinking that the operator had to watch a meter and power the motors manually but if I understand you correctly the motors would auto tune the antenna using an algorithm. this is pretty…
  • D_Hersey
    0 D_Hersey over 11 years ago

    I think due to its scale that this was used on the transmit side to normalize the load.  The application circuit would have been along these lines:

     

    Pi-Match | Electronics and Electrical Engineering Tools | EEWeb Community

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago

    'course, if you are going to dynamically adjust, you sorta need a reflectometer, https://en.wikipedia.org/wiki/Time-domain_reflectometer

    and a feedback loop.  One gotcha is that with the servo-system, you can space and not realize your antenna is icing until a critical point.  There is a corollary situation with automatic systems on wing flaps and icing in aviation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<