Passive Components
  • Technologies
  • More
Passive Components
Forum Peltier Cooling Module Data sheet understanding
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 111 subscribers
  • Views 4110 views
  • Users 0 members are here
Related

Peltier Cooling Module Data sheet understanding

e14 Contributor
e14 Contributor over 10 years ago

I am working on a project which envolves the implementation of Peltier modules. I am a mechanical engineering student. Currently, I am dealing with a Peltier cooling Module whose data sheet is shown below in the link from Farnell UK. We have Peltier cooling modules in the project which are supposed to cool down some flowing air. This is the first time I encounter Peltier modules.

http://www.farnell.com/datasheets/1693164.pdf

 

1-

I would like to ask about any good books available on the Thermo-electric effect, and more particularly Peltier modules, the physics behind them, mathematical models of them and their implementation.

 

2-

Also I would like to ask about the performance graph of the Peltier module (see the link below). According to what I understood from the explanation available on the Internet, the Pc notation on the graph refers to the cooling power. Is it the rate at which heat energy is absorbed on the cold side ??

 

3-

There is a heat little heat exchanger which consists of a heat sink, which holes filled in it and pipes are connected to flow water through the heat sink to increase the convective heat loss and prevent any overheat. While Tc the temperature on the cold side, can Th be considered as the ambient temperature ?

 

http://oi57.tinypic.com/34hj2m8.jpg

 

4-

On the performance graph, the "Th" at which the data in the graphs were collected is noted to be 25 C. Does this mean that I can refer to the graphs only in case that that the temperature on the hot side at that temperature ??

 

This because I found some sources on the Internet claiming at an offset of ±10 C, with a slight margin of error.

 

 

5-

The other thing I need to understand is that if my understanding of the cooling power "Pc", and if the temperature on the hot side "Th" remains constant as shown on the graph, for a given value of current as shown with the ascending lines on the right side in the lower section of the graph, why would the cooling power (the power absrobed on the cold side) fall if the temperature on the cold side falls as well. If my understanding of the cooling power is correct, then wouldn't the temperature of the cold side drop as more power "Pc" is absrobed ??

 

 

6-

In the lower section of the graph, if I choose two different intersection points on the straight line of the current value 4.8 Amp, when at "Tc = -20 C & Pc = 40 W" and when at "Tc = -5 C & Pc = 60 W", the corresponding temperature differential "dT" between "Tc" and "Th" is "45 C" and "30 C" in relation to the "Th" shown on the graph respectively. Thus, on the upper section of the graph, on the current line of 4.8 Amp, the intersection of the line with "dT= 45 C" & "dT= 30 C", yields voltage values of "V= 24.5 volts" & "V=23.5 volts" respectively. How can the same amount of current, and slight difference in voltage create a substantial difference in the temperature on the cold side ??

 

 

7-

How can I start with the implementation of the Peltier module, as I need a starting point. According to what I understood, I need to specify the temperatures I need on both sides of the module, with the cooling power (the power to be absorbed on the cold side, if my understanding of the cooling power shown on the graph is correct), so that I can specify the electric current value I need. Based on the temperature differetial between the hot and the cold side, and the value of the current, I can then determine the value of voltage I need to supply to the Peltier module, so that it generates the difference in temperature I need. Am I on the right track, and is there any piece of advise that I can make use of ??

 

 

Sorry for the very long thread.

 

Thanks in Advance

 

Regards

Attachments:
image
image1693164.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 10 years ago in reply to e14 Contributor +3 suggested
    The upper set of curves in your graph are telling you how the voltage cross the device will vary for each of 5 constant currents as the temperature difference across the device is varied. ie - the variation…
  • gadget.iom
    gadget.iom over 10 years ago +1 suggested
    This page may answer some of your questions: TEC / Peltier Element Design Guide | Compendium
  • michaelkellett
    michaelkellett over 10 years ago +1
    Your link doesn't lead to a picture but to some website requiring clicking and who knows what else. If you insert your picture directly into your E14 post I'll be able to look at it. Did you get the information…
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    Am 21.10.2015 um 22:24 schrieb Banshee For:

    I am working on a project which envolves the implementation of Peltier

    modules. I am a mechanical engineering student. Currently, I am dealing

    with a Peltier cooling Module whose data sheet is shown below in the

    link from Farnell UK. We have Peltier cooling modules in the project

    which are supposed to cool down some flowing air. This is the first time

    I encounter Peltier modules.

    http://www.farnell.com/datasheets/1693164.pdf

    (https://mail.yandex.com/re.jsx?h=a,ggFabqW2FW_fTrpozMU2CQ&l=aHR0cDovL3d3dy5mYXJuZWxsLmNvbS9kYXRhc2hlZXRzLzE2OTMxNjQucGRm)

     

    1-

    I would like to ask about any good books available on the

    Thermo-electric effect, and more particularly Peltier modules, the

    physics behind them, mathematical models of them and their

    implementation.

     

    2-

    Also I would like to ask about the performance graph of the Peltier

    module (see the link below). According to what I understood from the

    explanation available on the Internet, the Pc notation on the graph

    refers to the cooling power. Is it the rate at which heat energy is

    absorbed on the cold side ??

     

    3-

    There is a heat little heat exchanger which consists of a heat sink,

    which holes filled in it and pipes are connected to flow water through

    the heat sink to increase the convective heat loss and prevent any

    overheat. While Tc the temperature on the cold side, can Th be

    considered as the ambient temperature ?

     

    http://oi57.tinypic.com/34hj2m8.jpg

    (https://mail.yandex.com/re.jsx?h=a,Ve6XfGxq9DeW05E65tYxrQ&l=aHR0cDovL29pNTcudGlueXBpYy5jb20vMzRoajJtOC5qcGc)

     

    4-

    On the performance graph, the "Th" at which the data in the graphs were

    collected is noted to be 25 C. Does this mean that I can refer to the

    graphs only in case that that the temperature on the hot side at that

    temperature ??

     

    This because I found some sources on the Internet claiming at an offset

    of ±10 C, with a slight margin of error.

     

     

    5-

    The other thing I need to understand is that if my understanding of the

    cooling power "Pc", and if the temperature on the hot side "Th" remains

    constant as shown on the graph, for a given value of current as shown

    with the ascending lines on the right side in the lower section of the

    graph, why would the cooling power (the power absrobed on the cold side)

    fall if the temperature on the cold side falls as well. If my

    understanding of the cooling power is correct, then wouldn't the

    temperature of the cold side drop as more power "Pc" is absrobed ??

     

     

    6-

    In the lower section of the graph, if I choose two different

    intersection points on the straight line of the current value 4.8 Amp,

    when at "Tc = -20 C & Pc = 40 W" and when at "Tc = -5 C & Pc = 60 W",

    the corresponding temperature differential "dT" between "Tc" and "Th" is

    "45 C" and "30 C" in relation to the "Th" shown on the graph

    respectively. Thus, on the upper section of the graph, on the current

    line of 4.8 Amp, the intersection of the line with "dT= 45 C" & "dT= 30

    C", yields voltage values of "V= 24.5 volts" & "V=23.5 volts"

    respectively. How can the same amount of current, and slight difference

    in voltage create a substantial difference in the temperature on the

    cold side ??

     

     

    7-

    How can I start with the implementation of the Peltier module, as I need

    a starting point. According to what I understood, I need to specify the

    temperatures I need on both sides of the module, with the cooling power

    (the power to be absorbed on the cold side, if my understanding of the

    cooling power shown on the graph is correct), so that I can specify the

    electric current value I need. Based on the temperature differetial

    between the hot and the cold side, and the value of the current, I can

    then determine the value of voltage I need to supply to the Peltier

    module, so that it generates the difference in temperature I need. Am I

    on the right track, and is there any piece of advise that I can make use

    of ??

     

     

    Sorry for the very long thread.

     

    Thanks in Advance

     

    Regards

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/163918

     

     

    This is certainly the wrong  forum place for your questions.

    This is the  eagle forum and here we discuss problems and possibilities

    about the  eagle CAD software.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to autodeskguest

    Dear Mr. Joern

     

    I am so sorry for this, mistake, I just did not notice that I was posting in the wrong place. I just clicked on the "Start a Discussion" button on the home page, as I found some difficulities surfing my way in the website.

     

    Who can I contact (an admin or moderator) who may be capable of helping me to move this thread/discussion to the right section ?

     

    Thnaks for your reply and notice, and sorry for the very late reply, as I have been very busy lately.

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi Banshee,

    I will ask element14jamie to move your question to a better group.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • element14jamie
    0 element14jamie over 10 years ago in reply to jw0752

    Hello Paul,

    Thank you I have moved this to Passive area

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • element14jamie
    0 element14jamie over 10 years ago in reply to jw0752

    Hello Paul,

    Thank you I have moved this to Passive area

     

    Jamie