Passive Components
  • Technologies
  • More
Passive Components
Forum Overvoltage protection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 8 answers
  • Subscribers 111 subscribers
  • Views 2031 views
  • Users 0 members are here
Related

Overvoltage protection

e14 Contributor
e14 Contributor over 10 years ago

I have a problem with a variable ac wind generator

(15kW) which keeps blowing rectifiers. It normally generates at 300-350 v but can on a gust momentarily go over 400 which is the limit on the rectifiers which feed the inverters for onward network transmission.  I have rigged up, using a crouzet voltage control relay linked to a contactor, a bypass to protect inverters but it occurs to me that a capacitor bank or super cap would be able to 'absorb' the gust energy so;

am i correct in this assumption? if no, any suggestions for alternatives.  If yes, how do we size them and are we talking series or parallel? What would be the likely pitfalls/adverse consequences?!

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor +2
    current flow in windings is already near max on the gusts That does tend to limit your options a little. As I understand you can't reduce the load as that will tend to overspeed the blades, resulting…
  • jw0752
    jw0752 over 10 years ago +1 suggested
    Hi Ken, I know very little about wind mills but it seems to me that adding mass to the rotor would slow the reaction to wind gusts and even store some of the energy from the gust and spread it out over…
  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor +1 suggested
    Hi Ken, I do not see the capacitors as a solution to your problem. They would have to be on the rectified side of the diodes so they would actually be an increase in load at the time of stress. One solution…
Parents
  • jw0752
    0 jw0752 over 10 years ago

    Hi Ken,

    I know very little about wind mills but it seems to me that adding mass to the rotor would slow the reaction to wind gusts and even store some of the energy from the gust and spread it out over time. Also do you have a way to adjust the field of the alternator so that it can regulate the output voltage? If you are running with voltage close enough to the tolerance of your output circuitry that gusts of wind cause failure there may be something wrong with the design or the adjustment. As I mentioned I am not familiar with the specifics of windmills but just looking at your question from a peripheral understanding.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 10 years ago

    Hi Ken,

    I know very little about wind mills but it seems to me that adding mass to the rotor would slow the reaction to wind gusts and even store some of the energy from the gust and spread it out over time. Also do you have a way to adjust the field of the alternator so that it can regulate the output voltage? If you are running with voltage close enough to the tolerance of your output circuitry that gusts of wind cause failure there may be something wrong with the design or the adjustment. As I mentioned I am not familiar with the specifics of windmills but just looking at your question from a peripheral understanding.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jw0752

    Hi John, blades are 6 m long and 20m up in the air and all 'balanced' to spin at 90rpm so wouldnt want to mess with them.  It's a permanent magnet alternator, so no field coils to adjust. Newer models have wider voltage tolerance but it would cost thousands to change all the rectifiers/inverters so just looking for a more cost effective solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi Ken,

    I do not see the capacitors as a solution to your problem. They would have to be on the rectified side of the diodes so they would actually be an increase in load at the time of stress. One solution that I can see is to put an extra set of diodes in series or in parallel with your existing diodes. If you feel that it is the voltage that is killing the diodes put an extra set in series with the existing set. This will double the voltage specification. If you feel that it is the current that is killing them put the extra set in parallel with the existing set. This will double the current capacity of the system. Without pictures or more information I am not sure how this would work mechanically but from the point of view of the electronics it should work.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer