Passive Components
  • Technologies
  • More
Passive Components
Forum Higher capacitance but the same voltage.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 109 subscribers
  • Views 1238 views
  • Users 0 members are here
  • capacitor
Related

Higher capacitance but the same voltage.

czar9577
czar9577 over 9 years ago

Hello experts in electronics,

 

My queries are can I use a higher capacitance but the same voltage capacitor in my speedometer cluster gauge?  Like a 10 uF 25 volt capacitor replacing a 6.8 uF 25 voltage capacitor?

 

Thank you in advance.

 

Lou

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Lou,

    It will depend on how the capacitor is being used. If it is part of an averaging circuit then the answer is no. The capacitance change may change the input to output ratio and the speedometer may read too high. It is usually acceptable in circuits where the capacitor is being used as a filter to use a larger capacitance and the same or higher voltage. Remember that the voltage listed is just the limit of what the capacitor can tolerate before it begins to fail. Can you supply a schematic of the speedometer so we can see how the capacitor is being used?

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 9 years ago

    Hi Lou,

    It will depend on how the capacitor is being used. If it is part of an averaging circuit then the answer is no. The capacitance change may change the input to output ratio and the speedometer may read too high. It is usually acceptable in circuits where the capacitor is being used as a filter to use a larger capacitance and the same or higher voltage. Remember that the voltage listed is just the limit of what the capacitor can tolerate before it begins to fail. Can you supply a schematic of the speedometer so we can see how the capacitor is being used?

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer