Passive Components
  • Technologies
  • More
Passive Components
Forum Capacitance inversely proportional to voltage?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 111 subscribers
  • Views 4501 views
  • Users 0 members are here
  • capacitance measurement
  • capacitance
Related

Capacitance inversely proportional to voltage?

salesm21
salesm21 over 8 years ago

I just cant fathom why capacitance is inversely proportional to voltage. Maybe its my understanding of voltage or lack thereof. Voltage is the difference of potential energy between two points. 1 volt is equal to the force required to move 1 coulomb of charge past an arbitrary point in 1 second. So voltage measures how much energy is imparted to each coulomb of charge. Capacitance is when a dielectric keeps oppositely charged plates from equalizing there EMF. The formula for capacitance is C=Q/V. The Q I get because the more charge you have on either plate the more capacitance you will have. Voltage is the force that drives the charges apart. Some help in clarifying this would be great.

V/R

Sales

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +6 verified
    An analogy is water in a bucket - the bucket being the capacitor and the water is the charge. The voltage is the water depth. If you make the diameter of the bucket bigger (bigger capacitor) the same amount…
  • dougw
    dougw over 8 years ago in reply to salesm21 +1
    Correct. Q=CV so increasing either voltage or capacitance will increase the charge.
  • NigelB
    NigelB over 8 years ago in reply to salesm21 +1 suggested
    You seem to have forgotten that it is 1/Ct on the left hand side. So for example if you had two huge capacitances of 0.5 and put them in series, the equation would go: 1/Ct = 1/0.5 +1/0.5 = 2 + 2 = 4 which…
  • dougw
    0 dougw over 8 years ago

    An analogy is water in a bucket - the bucket being the capacitor and the water is the charge.

    The voltage is the water depth.

    If you make the diameter of the bucket bigger (bigger capacitor) the same amount of water (charge) will have a lower depth (voltage).

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • salesm21
    0 salesm21 over 8 years ago in reply to dougw

    So is this having to do with the fact that a bigger plate area will increase the amount of charge it can hold without applying any more pressure?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to salesm21

    Correct. Q=CV so increasing either voltage or capacitance will increase the charge.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • salesm21
    0 salesm21 over 8 years ago in reply to dougw

    Another question that's got me perplexed is perhaps more mathematical. I am trying to find the Ct in a series circuit with nothing but capacitors. The equation is 1/Ct=1/C1+1/C2...... However I noticed that most capacitors have values that are less that 1. AKA dividing a whole number by a number less than that will yield a larger number. Since in series capacitors are supposed to be inversely proportional this confuses me. Any help would be great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • NigelB
    0 NigelB over 8 years ago in reply to salesm21

    You seem to have forgotten that it is 1/Ct on the left hand side.

     

    So for example if you had two huge capacitances of 0.5 and put them in series, the equation would go:

     

    1/Ct = 1/0.5 +1/0.5 = 2 + 2 = 4

     

    which gives Ct = 1/4 = 0.25

     

    So Ct is lower even though you are adding two large numbers, as the large numbers are adding up to 1/Ct not to Ct, and the reciprocal of a large number is a small one (and vice versa, as you correctly observed)

     

    I hope that helps

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer