Passive Components
  • Technologies
  • More
Passive Components
Forum How to test this transformer?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 6 answers
  • Subscribers 110 subscribers
  • Views 3700 views
  • Users 0 members are here
  • samsung
  • tm-09175
  • syncmaster
  • t240
  • t-240
Related

How to test this transformer?

sebnast
sebnast over 6 years ago

Hi, I need help testing an inverter board transformer, I don't have much experience with this type of transformer and I'm not sure how to test it, I will be forever grateful for any suggestions.

the part is: TM-09175

photo attached.

 

Thanks

Seb

image

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 6 years ago +3 suggested
    Looking at https://www.badcaps.net/forum/showthread.php?t=54410 , a few entries in has testing process for this inverter: I would recap the board. You can also have worn out lamp so it draws too much current…
  • dougw
    dougw over 6 years ago +2 suggested
    Do you suspect the transformer is damaged? I don't know anything about this type of transformer so the following is just general transformer testing... First thing to do is a close visual inspection to…
  • jw0752
    jw0752 over 6 years ago in reply to sebnast +2 verified
    Hi Sebastian, I can see in your picture that there is an indication of wire and blue potting material in the wire channels on the two upper sets of contacts. I would expect to see some continuity between…
Parents
  • dougw
    0 dougw over 6 years ago

    Do you suspect the transformer is damaged?

    I don't know anything about this type of transformer so the following is just general transformer testing...

    First thing to do is a close visual inspection to see if all the windings and insulation are intact without nicks, pitting, dents or shorts and no signs of overheat (charring & discoloration).

    Next measure resistance between the 2 coils - I don't think they should be shorted together.

    Next measure the resistance of each coil - they should be very low resistance - not open circuit.

    You can try measuring the inductance of each coil to get some idea of the number of turns.

    You could try applying a low-voltage, current-limited oscillation signal to the primary (the coil with fewer turns and heavier wire) and see if the secondary has the appropriate step up voltage.

    If it is operating in its normal circuit, you can measure its temperature.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sebnast
    0 sebnast over 6 years ago in reply to dougw

    One of the possibilities yes as for the test the two pins attached to the braided wire are shorted and the rest has no relation to any other, it's all open line. (see photo)image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to sebnast

    I can't tell from the picture, but is there actually any wire in the cores at either end?

    It looks like there are channels for wire to come to the pins, but there is no wire coming to the pins...

    It looks like all the turns of braided wire are touching, which would mean there is no coil. Is this the case, or are all the strands coated with enamel?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to sebnast

    Hi Sebastian,

     

    I can see in your picture that there is an indication of wire and blue potting material in the wire channels on the two upper sets of contacts. I would expect to see some continuity between there connections at the top of your picture. It is unusual for transformers like this to fail. It would be even more unusual for the two side coils to both fail. Make sure you check all the combinations of the 4 upper connectors to see if they have made the connections in a less than obvious manner. If the upper connectors are indeed open then you have a failed component.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sebnast
    0 sebnast over 6 years ago in reply to jw0752

    Hi, thanks for all the answers guys, you're right I've had another look and both coils (thin wire) have around 1K between the pins the middle coil (multicore spun wire) has continuity between the pins.

    Is that expected behaviour please?

     

    Seb

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to sebnast

    Yes that sounds normal.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 6 years ago in reply to sebnast

    Yes that sounds normal.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • sebnast
    0 sebnast over 6 years ago in reply to jw0752

    thank you.