Passive Components
  • Technologies
  • More
Passive Components
Forum Information on the clear connection film to an LCD display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 23 replies
  • Answers 16 answers
  • Subscribers 110 subscribers
  • Views 10539 views
  • Users 0 members are here
  • lcd_connection
Related

Information on the clear connection film to an LCD display

jw0752
jw0752 over 6 years ago

I have recently been asked by a friend andriu011   how to improve the connection of the clear film ribbon between a glass LCD display and a circuit board. Frankly I do not even know the technical name of this type of connection cable. I have seen them and been frustrated by them when they have lost their connection. Usually pressure is applied to the back of the film against the glass to make the connection to the LCD circuits in the glass. If anyone knows what to call this technology so I can google it and learn more it would be appreciated. Also if you have any suggestions for cleaning the connections or improving them please tell me.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • andriu011
    andriu011 over 6 years ago +4 suggested
    Thank you John for putting this post up, also thank you everyone for any help and great recommendations, the display looses the segments of the numbers and within time all the segments go away, i have…
  • andriu011
    andriu011 over 6 years ago in reply to beacon_dave +4 suggested
    Yes, the end attached to the glass seem attached strongly, i am heating and press pressure to the end cable that is attached to PCB. Here is another picture with same remote but something black stuff added…
  • andriu011
    andriu011 over 6 years ago in reply to jw0752 +3 suggested
    Hi John, Here is the picture of the remote.
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to andriu011

    Aw Andrei, I have had LCDs with flat flex issues too.

    I have been able to temporarily fix issues by bending them in a position where they made the LCD work, then taping everyting with normal bureau tape. But that never lasts.

     

     

    Otherwise, merely glueing it won't work I think, since there is nothing to apply pressure to each contact along the plastic.

     

    You're supposed to use a hot bar (a very very broad soldering iron, as long as the flat flex and as broad as the solder-down contacts). Tricky.

    The display looks like the Nokia one used on the older TI MSP320 LCD boosterpack (used it in the first design of the eLoad here on e14). I believe there is no stock left of the source LCD - one of the reasons that the boosterpackis obsolete now.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • andriu011
    0 andriu011 over 6 years ago in reply to beacon_dave

    Dave, if i get this 3M you mentioned above, getting the model ACF 7303, i am not sure how wide is the roll but if i cut it to be the size of the zebra line that is on my remote and glue each line one by one will that be an option. My thinking is if that tape has strong glue and can stick great that might fix the issue potentially. What do you think? Thank you

     

    3M ACF 7303

     

     

     

    3M ACF 730

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 6 years ago in reply to andriu011

    Adafruit supplies it as a 50mm x 150mm patch (see Shabaz's link).

    3M appear to supply it in 32.9m rolls of varying widths.

     

    You wouldn't have to cut it line by line as it is 'anisotropic', otherwise you could just use conductive tape. You just need a single strip that covers the area of the ribbon that is in contact with the PCB.

     

    It will depend a lot on how cleanly you can separate the existing join. It is an adhesive solution so you are basically replicating what you already have.

     

    You may still want to investigate some mechanical method over and above the adhesive. 3M recommend using it in conjunction with this tape.

     

    Does the display start working with manual pressure applied in its current configuration ? If so it may be worth looking at a mechanical clip solution first.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<