Passive Components
  • Technologies
  • More
Passive Components
Forum Problem of boost converter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 111 subscribers
  • Views 891 views
  • Users 0 members are here
Related

Problem of boost converter

e14 Contributor
e14 Contributor over 15 years ago

Hello everyone, please help...

 

When i connect the circuit as the schematic below: the output is not changeable which means when I alter my Pot, the output remains the same. ( the frequency is about 2.3Khz)

One thing that I have observed is, the output is now depending on my Inductor value.

1mH = 100V++;10mH= 51V.

I burned my 3mH inductor while I was using C1=47uF (last time, the inductor wasn't burned !!! I wonder why)

The duty cycle is about 60%.

Things that I've summarized are :
1. When switching frequency is up to 23kHz, the inductor is alright but  the output is not alterable; When switching frequency is low as 1.4kHz,  the output can be altered but inductor will be burst ( it's like  overheat and cause the outside(cover) of the coil inductor melts.)

2. The feedback system seems like failure when frequency is as high as 20kHz. But, why?

3.  For 1 &2 are the conditions under resistor as load. And, I just  connected it to the real load that I wanted to connect. Things happen:
image The output voltage was less than just now: for 10mH, it became 30V;for 1mH, it became 80V [the output voltage is less 20V compare the just now]
(ii) When I connected to 1mH inductor, both of the inductor and Mosfet is quite hot ( i just connect it about 10++min)

4. "Hiss" sound is gone when the switching frequency is 20kHz with 60%duty cycle; "hiss" sound appears when switching frequency is 1.4kHZ...

Does anyone have any ideas regarding my problem? What should I do? Thanks a lot in advanced.

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Sorry, the C1 should be 2.2nF. and R1 is 3k Ohms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    anyone could help?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    anyone could help?