Passive Components
  • Technologies
  • More
Passive Components
Forum time delay relay alternative?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 2 answers
  • Subscribers 111 subscribers
  • Views 3791 views
  • Users 0 members are here
  • relay
Related

time delay relay alternative?

e14 Contributor
e14 Contributor over 11 years ago

Hello,

 

I'm trying to set up a relay that will ignore short spikes in the control signal.  Specifically, I'd like to activate the relay when a signal is at least 10 seconds long, but ignore anything shorter.  I know I can do this with a delay on make relay, but it seems overkill for what I want to do.  Are there any simpler alternatives?  I don't need to adjust the delay time - a fixed delay would be fine.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Craigt; I had some extra time today so I bread boarded a circuit to delay the actuation of a relay for 10 seconds from the time power is applied to the circuit. Here are a couple pictures and a schematic…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    John, John, John.  Let's put a CL resistor in the base lead of the Q.  Otherwise, you are shorting the output stage of the 555 to .6V.  Survivable for a 'C555, but nasty.

     

    The 'thresh' terminal can be grounded.  Thresh is a comparator set at 2/3 Vcc for turning off the F/F.  We never intend to turn off the F/F, in this design as John proposes it.  If this circuit works, which I take on faith, Trig dominates Thresh, which is just a peculiarity of the F/F, not that it matters.

     

    The time delay here is, presuming the cap is initially discharged, the wait for RC to reach (neglecting latencies) 1/3 VCC .  Another idea would be to trigger the 555 on power up using a small RC, than use a big RC to reset the thing via Thresh.  This would give us a crossing-point at 2/3 Vcc for more bang-for-buck out of our timing components, and relieving us from worrying about our device triggering on pwr-up, because we intend for it to.

     

    RC time constant / voltage calcultor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to D_Hersey

    Don is most certainly correct and thankfully sees the flaws in my circuits and corrects me. We should add a resistor between the #3 pin output of the 555 and the base of the transistor to limit the current draw on the 555. I put a 1K into my test circuit and it worked the same way. Since this is a design that I got from the 555 circuit book listed above I am not sure what Don means by wanting the #6 Thresh pin tied to ground. I will have to experiment with this tonight to see what that does. The current analysis is that the circuit works as drawn but the insertion of a 1K resistor between the #3 pin of the 555 and the base of the transistor is a very good idea.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to D_Hersey

    Don is most certainly correct and thankfully sees the flaws in my circuits and corrects me. We should add a resistor between the #3 pin output of the 555 and the base of the transistor to limit the current draw on the 555. I put a 1K into my test circuit and it worked the same way. Since this is a design that I got from the 555 circuit book listed above I am not sure what Don means by wanting the #6 Thresh pin tied to ground. I will have to experiment with this tonight to see what that does. The current analysis is that the circuit works as drawn but the insertion of a 1K resistor between the #3 pin of the 555 and the base of the transistor is a very good idea.

    John