Passive Components
  • Technologies
  • More
Passive Components
Forum time delay relay alternative?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 2 answers
  • Subscribers 111 subscribers
  • Views 3803 views
  • Users 0 members are here
  • relay
Related

time delay relay alternative?

e14 Contributor
e14 Contributor over 11 years ago

Hello,

 

I'm trying to set up a relay that will ignore short spikes in the control signal.  Specifically, I'd like to activate the relay when a signal is at least 10 seconds long, but ignore anything shorter.  I know I can do this with a delay on make relay, but it seems overkill for what I want to do.  Are there any simpler alternatives?  I don't need to adjust the delay time - a fixed delay would be fine.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Craigt; I had some extra time today so I bread boarded a circuit to delay the actuation of a relay for 10 seconds from the time power is applied to the circuit. Here are a couple pictures and a schematic…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    If the reset pin isn't asserted on 555, a signal below 1/3 Vcc on Trig sets the F/F and a signal greater than 2/3 Vcc on Thresh resets it.  It seems Trig dominates Thresh.  If this doesn't make sense, read about set/reset dominated flip-flops on google.  The combination of two comparators, a three-resistor string and a flip-flop is a very common occurrence in analog, the 555 is a great idea!  John is a great spirit and always accepts my chiding with good humor.  I try to twit him, but it never avails.

     

    http://www.ti.com/lit/ds/symlink/lm111-n.pdf

     

    The 311 comparator works up to 36V, if we use it, we won't need the VR, not that it a bad idea.  Look at example #50.  The output stage of the comparator is open-collector NPN.  So they are using it to drive a PNP output transistor, forming a http://en.wikipedia.org/wiki/Sziklai_pair.

     

    The input stage works to slam the output stage based on the differential input - the offset voltage.  Gain is very high, but there is a small zone of metastability.  To repeat, if the + input is slightly higher than the - input the output slams high, if the - input is slightly higher than the + input it slams low.  Input range is a consideration with comparators.

     

    We can make a string of a resistor (the 'ballast') and a backwards Zener and hook them across the supply to provide a reference, or we can just use a 2R string.  This would go to one input of our comparator, the other input would be attached to the tap of the timing RC across the supply.  When C charges past the threshold-we switch.  We might hook up a very large resistor (small conductor) from the output of the comparator to the + input (for example) to keep our circuit from chattering.  This is a form of a 'Schmidt trigger,' which removes the metastability.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    If the reset pin isn't asserted on 555, a signal below 1/3 Vcc on Trig sets the F/F and a signal greater than 2/3 Vcc on Thresh resets it.  It seems Trig dominates Thresh.  If this doesn't make sense, read about set/reset dominated flip-flops on google.  The combination of two comparators, a three-resistor string and a flip-flop is a very common occurrence in analog, the 555 is a great idea!  John is a great spirit and always accepts my chiding with good humor.  I try to twit him, but it never avails.

     

    http://www.ti.com/lit/ds/symlink/lm111-n.pdf

     

    The 311 comparator works up to 36V, if we use it, we won't need the VR, not that it a bad idea.  Look at example #50.  The output stage of the comparator is open-collector NPN.  So they are using it to drive a PNP output transistor, forming a http://en.wikipedia.org/wiki/Sziklai_pair.

     

    The input stage works to slam the output stage based on the differential input - the offset voltage.  Gain is very high, but there is a small zone of metastability.  To repeat, if the + input is slightly higher than the - input the output slams high, if the - input is slightly higher than the + input it slams low.  Input range is a consideration with comparators.

     

    We can make a string of a resistor (the 'ballast') and a backwards Zener and hook them across the supply to provide a reference, or we can just use a 2R string.  This would go to one input of our comparator, the other input would be attached to the tap of the timing RC across the supply.  When C charges past the threshold-we switch.  We might hook up a very large resistor (small conductor) from the output of the comparator to the + input (for example) to keep our circuit from chattering.  This is a form of a 'Schmidt trigger,' which removes the metastability.