Passive Components
  • Technologies
  • More
Passive Components
Forum time delay relay alternative?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 2 answers
  • Subscribers 111 subscribers
  • Views 3800 views
  • Users 0 members are here
  • relay
Related

time delay relay alternative?

e14 Contributor
e14 Contributor over 11 years ago

Hello,

 

I'm trying to set up a relay that will ignore short spikes in the control signal.  Specifically, I'd like to activate the relay when a signal is at least 10 seconds long, but ignore anything shorter.  I know I can do this with a delay on make relay, but it seems overkill for what I want to do.  Are there any simpler alternatives?  I don't need to adjust the delay time - a fixed delay would be fine.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Craigt; I had some extra time today so I bread boarded a circuit to delay the actuation of a relay for 10 seconds from the time power is applied to the circuit. Here are a couple pictures and a schematic…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Craigt;

    I had some extra time today so I bread boarded a circuit to delay the actuation of a relay for 10 seconds from the time power is applied to the circuit. Here are a couple pictures and a schematic.

     

                imageimageimage

     

    If you click on the images they will enlarge. I had to actually use 2 resistors on the breadboard to get the required 80K to make the unit trigger at 10 Seconds.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    Hi John,

     

    Wow, the amount of effort you have put into helping me is completely unexpected.  Thank you.

     

    I did read the question from Nick123 before posting, but thought that my application was slightly different and I did not want to divert the focus in his thread.

     

    Do you know of any pre-packaged 555 applications for common delay lengths?  I'm looking for something that can be used in an industrial setting, so enclosed akin to a typical plug-in relay.  I'll be using a 24 VDC signal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi Craigt,

    The 555 is just a chip and the delay is selectable by the choice of R1 and C1 in my schematic. There are no plug in modules at a reasonable price though I am sure there are some multi function 24 V time delay relays available for industrial applications. The 24 volt input that you mention would require us to put some sort of simple voltage regulator on the 555 as it is limited to 15VDC max. It does, at this point, sound like your application would be fairly easy to adjust to but if you have no experience you may want to get an engineer or a technician to help with the design. Any ideas or design ideas that I put out on this thread are free for you to use but If you are going to use them for any critical process you must get verification from an engineer that they adequate for what you want to do and will work in your industrial setting. Anyone who is going to put a design together will need all the parameters of the application so they know the voltage going in and how big a load you are controlling as well as any other important aspects. You will also have to decide how you want the system to respond to different inputs. For example the circuit that I have drawn will respond to an 11 second input pulse with 1 second of relay actuation. Is this what you are looking for? There are often many solutions for a particular problem but the resolution will start with a good picture of your operational parameters and a clear description of your goals. Keep us posted how you are progressing.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    The 555 circuit looks like a fun project to try when I've got the time.  But for my needs at the moment I'm going to stick with a standard time delay relay.

     

    Thank you for the help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    The 555 circuit looks like a fun project to try when I've got the time.  But for my needs at the moment I'm going to stick with a standard time delay relay.

     

    Thank you for the help.