Passive Components
  • Technologies
  • More
Passive Components
Forum Colpitts Crystal Oscillator Circuit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 1 answer
  • Subscribers 112 subscribers
  • Views 8581 views
  • Users 0 members are here
  • crystal
  • colpitts
  • oscillator
Related

Colpitts Crystal Oscillator Circuit

jw0752
jw0752 over 11 years ago

In the last couple days I have been experimenting and learning about crystal oscillator circuits. I am doing this with no particular application in mind. I have been able to get a couple circuits to work as expected but there is one circuit that I got from the book " Practical Electronics for Inventors" by Paul Scherz and Simon Monk that I have not been able to get working. I have tried different transistors and I have tried varying the values of the support passives. I am wondering if anyone has had experience with this circuit and can give me a hint as to where to look for my failure to get it to work. There is also one other possibility. This book has been known to include errata from time to time so I wouldn't be completely surprised if there is something wrong with the circuit. Any insights would be appreciated.

 

John

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago +1 verified
    Thanks for bringing up the interesting topic, I had some fun experimenting briefly. This was the circuit I tried, it works (well, it oscillates) although I have no idea about the quality of the output…
  • jw0752
    jw0752 over 11 years ago in reply to shabaz +1
    Hi Shabaz, Wow you did an awesome job. I have so much fun just toying around with things like this and it is fun to find that there are others that can't resist figuring things out too. I will find a BF199…
  • D_Hersey
    D_Hersey over 11 years ago +1
    http://www.edn.com/design/sensors/4406691/3/Oscillators--How-to-generate-a-precise-clock-source http://www.edn.com/design/sensors/4429819/Crystal-Oscillator-Fundamentals-and-Operation-Part-II http://www…
Parents
  • shabaz
    0 shabaz over 11 years ago

    Hi John,

     

    I tried the circuit just now too, and experienced failure with it just like you. You're right, the circuit is incorrect, probably never tested. The reason is the transistor : ( According to the datasheet (I checked PN2222, which is the plastic version of the 2N2222, which is what I had), it has current gain-BW product of 300MHz, i.e. at 10MHz, the gain (AC small-signal gain) would be not higher than 30. However, this is not likely either, because this is spec'd at 20mA collector current according to the datasheet, so the actual gain will be lower still.

    I fiddled with the circuit before I realized this, and it still didn't work. However after swapping out with a BF199 (550MHz fT, spec'd at 5mA), it worked. However now my circuit is slightly different from yours. I'll draw it up, and then move the components on the breadboard back to the original circuit (but with BF199) to see if it still works.

    (I tested with a radio).

    However, as I understand, BF199 is a European transistor. Hopefully you can still get it easily in the US, otherwise an alternative is needed.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago

    Hi John,

     

    I tried the circuit just now too, and experienced failure with it just like you. You're right, the circuit is incorrect, probably never tested. The reason is the transistor : ( According to the datasheet (I checked PN2222, which is the plastic version of the 2N2222, which is what I had), it has current gain-BW product of 300MHz, i.e. at 10MHz, the gain (AC small-signal gain) would be not higher than 30. However, this is not likely either, because this is spec'd at 20mA collector current according to the datasheet, so the actual gain will be lower still.

    I fiddled with the circuit before I realized this, and it still didn't work. However after swapping out with a BF199 (550MHz fT, spec'd at 5mA), it worked. However now my circuit is slightly different from yours. I'll draw it up, and then move the components on the breadboard back to the original circuit (but with BF199) to see if it still works.

    (I tested with a radio).

    However, as I understand, BF199 is a European transistor. Hopefully you can still get it easily in the US, otherwise an alternative is needed.