Passive Components
  • Technologies
  • More
Passive Components
Forum Capacitor replacement
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 26 replies
  • Subscribers 112 subscribers
  • Views 4075 views
  • Users 0 members are here
Related

Capacitor replacement

e14 Contributor
e14 Contributor over 11 years ago

Hello everyone!

I would need your help solving a little problem where I am not sure of the value of a capacitor that I need to replace.

I have never seen a capacitor like this one (yep, I'm a noob) so I searched online for some info and I though I could read it's value...the problem is that when I desoldered it from the board I noticed that on the other side it had other things written that, to my little knowledge, suggest a different value. Here are the pictures:

 

image

From this one I read that the precision is B, and the value is 4.1 uF with max 400v. The rest of the letters I have no idea what they mean.

image

From this one I read that it is a 4,7 pF capacitor and the precision is M. The rest I do not understand.

 

What I would really like to know is what the actual value of the capacitor is and if possible, what the various things on both sides mean so that in the future I will be able to read them.

Thank you very much in advance

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago +1
    Typing 472M into google gives you 26,700 replies or thereabouts. http://www.csgnetwork.com/capcodeinfo.html Your out by a long way ... Why are you thinking that is the problem.? I'd be looking more at…
  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor +1
    Do you suggest replacing both the resistor and the capacitor at this point? Why? If the value of the capacitor (now you have it out) and the resistor are what they should be, then there is really no…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1 +1
    This is the main board from a 1970's/1980's tv...the power supply should be ok as it is a separate unit and I got it fixed a few months ago. The problem is that a few days ago the tv made a noise (like…
Parents
  • mcb1
    0 mcb1 over 11 years ago

    Typing 472M into google gives you 26,700 replies or thereabouts.

    http://www.csgnetwork.com/capcodeinfo.html

     

    Your out by a long way ...

     

    Why are you thinking that is the problem.?

    I'd be looking more at the component behind it, as it looks like either a scorch mark, or heat from a resistor.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    Ok, thank you very much! I though that was the problem because it is the only component that has any marks of damage, but it was right in front of a resistor so as you said it could probably be the heat from the resistor that made that mark. Do you suggest replacing both the resistor and the capacitor at this point?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to e14 Contributor

    Do you suggest replacing both the resistor and the capacitor at this point?

    Why?

    If the value of the capacitor (now you have it out) and the resistor are what they should be, then there is really no point.

     

    Looking at the dust and dirt I'm picking its a 5-10 year old device.

    Often the marks are often just discolouration from the dust getting hot and marking the item.

    Sometimes its poor design, where parts are okay under normal working, but as capacitors age, then they have to work much harder, and hence more heat is imparted onto adjacent parts.

     

     

    What is wrong with ???.

    Have you used google to search for a schematic.???

    Many of the power supply boards are common to several brands, so try to find some identifying marks on the board, and search using that.

     

    I doubt this is the cause of your problem.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    This is the main board from a 1970's/1980's tv...the power supply should be ok as it is a separate unit and I got it fixed a few months ago. The problem is that a few days ago the tv made a noise (like a little explosion), the power went out and it never turned on again... I opened it up and this was the only thing I found that had any marks of damage on it. Well, this and another component that I have no idea what it is and that I was going to search on google for if this capacitor did not solve the problem. The reason for not suspecting the other component is that all I can see is that the bottom of the board is darker under that component but the component itself doesn't seem to be damaged.

    Now I am going through all the parts in the tv, one by one, cleaning the dust and double checking each component for visual damage.

     

    The following is a picture of the area where the capacitor was:

    image

    The two red arrows indicate the main components to which the capacitor was connected.

     

    You can also see the resistor that was right in front of the capacitor, it's the vertical one right above the bottom arrow. Any suggestions on how to procede are welcome

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    This is the main board from a 1970's/1980's tv...the power supply should be ok as it is a separate unit and I got it fixed a few months ago. The problem is that a few days ago the tv made a noise (like a little explosion), the power went out and it never turned on again... I opened it up and this was the only thing I found that had any marks of damage on it. Well, this and another component that I have no idea what it is and that I was going to search on google for if this capacitor did not solve the problem. The reason for not suspecting the other component is that all I can see is that the bottom of the board is darker under that component but the component itself doesn't seem to be damaged.

    Now I am going through all the parts in the tv, one by one, cleaning the dust and double checking each component for visual damage.

     

    The following is a picture of the area where the capacitor was:

    image

    The two red arrows indicate the main components to which the capacitor was connected.

     

    You can also see the resistor that was right in front of the capacitor, it's the vertical one right above the bottom arrow. Any suggestions on how to procede are welcome

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    I like the picture of older things that were made to last. image image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to e14 Contributor

    main board from a 1970's/1980's

    So start searching for that....

     

    Once you have that you can start tracing to see where voltages aren't.

     

    Someone appears to have replaced at least two electrolytic capacitors .. so that's a start.

    The main board has some very high voltages, and they can easily cause some major damage ...so one hand in the pocket rule applies.

    The value of the capacitor and the transformer suggest its part of the flyback circuit.

    It might be damaged so check it with a meter, as this circuitry cannot generate lots of energy to explode things.

     

    I'd be hunting for transistor/fets that have pieces missing or the mounting hardware is dislodged.

     

    Out of curiousity why are you keen on saving this.?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    This might sound pretty dull but this is the first TV on which I started playing videogames and now I connected all the consoles that I managed to retrieve over the years and I am building a little cabinet that incorporates everything. I know it's an old TV and it might not be worth the effort but I'll do what I can to bring it back to life...not to mention it is a great TV and the quality is (was up until a few days ago) exceptional.

     

    The only schematics I could find are for sale and I'm not even sure they are the right ones. So I'll follow your advice and with a lot of patience I'll try to find out where the problem is. Thank you very much for your help. If it's ok with you, when I run into something I'll write here what I find

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to e14 Contributor

    The only schematics I could find are for sale

    Keep searching and don't be afraid if some are in the former USSR as they seem to have lots of circuits/schematics.

    Try the forums for the TV as often they link to circuits.

     

    You had the supply repaired ... is the shop that did that able to help.?

     

    Just post back here.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    Well the shop is probably capable of repairing the tv...the problem is that when I got the supply fixed I was very unhappy with the price. I know that many times people expect lower prices because they don't know how much time and effort it takes to repair this kind of stuff, but when I brought the TV I had already opened it and I told them where the problem was because it was very easy to spot. The only reason I brought the TV to them was because I didn't feel experienced enough to repair an old TV without risking to damage it. The point is, when I went back to get the TV, they charged me 80 bucks just to replace a capacitor. I don't find that to be fair since I know that it didn't take them much work...sorry for bothering you with this long story ahah

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    Ok, so, after some tinkering and testing I think I might have found the problem...but still, as I am used to, I have a doubt. Here is what I found.

     

    There is a transistor (pretty big one) that does not seem to have any visual damage on it but when I tested it I got the following results:

    pin 1 (positive lead multimeter) to pin 2 (negative lead multimeter) gave me the same resistance (almost, slightly higher) as pin 3 (positive lead multimeter) to pin 2 (negative lead multimeter) so I am thinking this is a PNP transistor,

    and since pin 1 to pin 3 gave me no resistance I am thinking the transistor is damaged.

    The "only" problem is that if I search for the code on the transistor (C3892A) on google I can only find datasheets for NPN transistors that go by that name.

    I am seriously confused right now. If you could give me some advice on this I would greatly appreciate it

     

     

    Here is the complete list of values from the multimeter:

     

    pin 1 (positive) to pin 2 (negative) reads 406;

    pin 1 (positive) to pin 3 (negative) reads 40 and beeps;

    pin 2 (positive) to pin 1 (negative) reads 1;

    pin 2 (positive) to pin 3 (negative) reads 1;

    pin 3 (positive) to pin 1 (negative) reads 40 and beeps;

    pin 3 (positive) to pin 2 (negative) reads 431;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to e14 Contributor

    Franceso.

    Really quick reply from the airport.

     

    Try searching for a 2SC3892A.

    They usually drop the 2S to save room.

     

     

    Most transistors don;t show well unless you can bias the base with a finger or resistance to force it to conduct.

    Robert Peter Oakes

     

    Peter can you help in my absence.....image

     

    cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi Francesco,

    Your transistor number does cross to an NPN deflection / flyback transistor. How are you determining the polarity of your test leads on your Ohm meter? Several of my meters have the positive voltage on the black lead of the Ohm meter. Confusing but for whatever reason this is the way they were designed. Typically these transistors fail in a shorted condition. If you do not have a short between any of the leads it may not be the transistor.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    Ok, thank you very much...by adding the "2S" in front I was able to find a lot of information on the transistor!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    The multimeter should be "regular" with red as positive and black as negative because all other readings suggest so and I was also able to power up an LED with the diode testing mode and that further suggested what the polarities are. Now, assuming it is a NPN transistor as the datasheets say, I built a tiny circuit giving +5volts to the Collector, ground to the emitter and when I put something around +3 volts on the Base the current went through (I powered an LED). I also am pretty sure of which is base, which collector and which emitter because they are printed on the board. The transistor seems to work fine with low voltages and currents, I don't know if it may behave differently when those currents are increased...this to me suggests that the problem is elsewhere.

     

     

    Ok, I just did another test...this time I assumed it was a PNP transistor. I connected +5v to the emitter, ground to the base and current went out the collector to power an LED. At this point I figured something was wrong so I disconnected ground from the base and it still powered the LED...I am afraid either I do not understand transistors that much (very very possible) or the transistor is working in weird ways