Passive Components
  • Technologies
  • More
Passive Components
Forum Hey, Guys, I'm stumped It
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 106 subscribers
  • Views 6927 views
  • Users 0 members are here
  • logo
  • resistor
  • manufacture
Related

Hey, Guys, I'm stumped It

phoenixcomm
phoenixcomm over 3 years ago

imageOk, it claims to be a 0.22Ω 3watt power sand resistor, with 3 legs. (so starting at the top and going clockwise, 1 at the top, 2 on the right, and 3 on the left)

My fluke 113 says no it's 0.38Ω between 1 and 2, as well as between 1 and 3, and 0.59/0.60Ω between 2 and 3. 

My HP3435A  set on the 20Ω scale says it's 0.37Ω between 1 and 2, and 0.38Ω between 1 and 3, and 0.59Ω/0.60Ω between 2 and 3.

Something is not right. 

and Please look at the logo, so I can figure out who made the stupid thing..

oh btw the wires go all the way through the body and are about 1" long on the reverse side. 

Thanks again. Cris

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 3 years ago +5
    As you've got two meters, perhaps just do your own four-wire measurement. Set a PSU to constant-current, use one of your meters to measure the current through the resistor, the other to measure the voltage…
  • beacon_dave
    beacon_dave over 3 years ago in reply to jc2048 +5
    Push pull amplifier designs appear to use them. Here is a Sony receiver design using a similar device. https://www.petervis.com/Amplifiers/sony-str-k740p/how-to-fix-sony-amplifier-protect-mode-error…
  • michaelkellett
    michaelkellett over 3 years ago +4
    Just guessing but: lets assume your leads have about .15 ohm resistance. then its a 0.22 R from 1 to 2, a second 0.22R from 1 to 3 (they both read about 0.37) so from 2 to 3 its 0.44R + the lead reistance…
Parents
  • dougw
    dougw over 3 years ago

    If you short 2 and 3 do you get 0.22 ohms between 1 and the short?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 3 years ago in reply to dougw

    I was thinking the same except I would suggest shorting pin 1 to pin 2.  This would put the 0.38 OHM resistance in parallel with the 0.6 OHM resistance which of course is very close to the 0.22 OHM.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dang74
    dang74 over 3 years ago in reply to dougw

    I was thinking the same except I would suggest shorting pin 1 to pin 2.  This would put the 0.38 OHM resistance in parallel with the 0.6 OHM resistance which of course is very close to the 0.22 OHM.