Passive Components
  • Technologies
  • More
Passive Components
Forum Dealing with Unexpected Emissions: The Fellowship of the Ferrite Ring
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 107 subscribers
  • Views 6122 views
  • Users 0 members are here
  • ferrite ring
  • MXO4
  • emc
  • MXO 4
  • spectrum analyzer
  • toroid
  • choke
  • oscillator
  • ferrite core
  • Fair-Rite
  • ferrite
  • inductor
Related

Dealing with Unexpected Emissions: The Fellowship of the Ferrite Ring

shabaz
shabaz over 3 years ago


I was experimenting with bits of circuit, hopefully, to become a power supply eventually. It is a work in progress.

At this stage, I’m using bits of scrap copper-clad board, each with a sub-module. It’s too early for a PCB.

image

However, during the prototyping, I noticed (amongst other issues that I need to solve!) a particular artifact on the ‘scope trace when looking at the output.

This situation ended up being a good example of where it pays to zoom out and look at a lot more of the spectrum view than expected!

Admittedly this was a lot easier to identify using the MXO 4 ‘scope, but it would be possible to spot with other test equipment, such as a spectrum analyzer and a near-field probe. I just used the normal 'scope probe, I didn't do anything special.

With the MXO 4, the anomaly was zoomed in, and then using a logarithmic-frequency spectrum view, it was possible to see the extent of the problem, with the left side of the spectrum view showing the wanted oscillation (fundamental frequency) and its harmonics, and the right side showing the spurious output.

image

Now I could try to do something about it!

I used tiny ferrite rings (legend has it they were forged by Fair-Rite, part code 2643001501 ) on the base input of the transistors. Essentially, they act as a bit of additional resistance for the higher frequencies. The rings cost $0.02 currently (although more expensive in the UK).

image


Back to the ‘scope:

image

Much better!

As mentioned, I still have other problems to deal with, but I thought it was a nice example of why it makes sense to do testing to frequencies far higher than expected, just in case there are spurious emissions, and why it can be a good idea to possess the rings because one never knows when they are needed.

Thanks for reading!

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to anniel747 +3
    or nail polish. Also good to fix broken-off enamel.
  • robogary
    robogary over 3 years ago +2
    nice. I wouldnt have looked that closely to notice the ring.
  • anniel747
    anniel747 over 3 years ago in reply to shabaz +2
    Or conventional varnish dip.
Parents
  • anniel747
    anniel747 over 3 years ago

    Schematic? Frequency response of the toroid used?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to anniel747

    I've tried several toroids so far (I didn't take photos or screenshots of them all, so the first PCB photo shows a different toroid to the last PCB photo! : ) because I wanted to use a commonly-available one so the circuit can be easily replicated. This was hard though, because in toroid form most ferrites are for chokes. As a result I'm seeing efficiencies barely approaching 50% at best so far, and quite an ugly waveform under load.

    I have ordered some hopefully more suitable ferrites to see if that can be improved, although I don't really mind if it is 50% efficient (I'm aiming for cheapness and low noise). 

    II only started on this yesterday, and the board is scratched-out copper-clad) but have already constructed perhaps 5 or 6 transformers, pulling off the windings and reattempting each time. I barely have any power toroids to experiment with here, although I have a fair amount of cores for chokes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 3 years ago in reply to shabaz

    Any specs on the chokes used? Those are pulls if understand correctly?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to anniel747

    Do you mean component pulls? No, I'm trying to use easily-available parts, to make it repeatable. It's just unfortunate that most of the toroids I have (all with a part code so they can be purchased) are lossy, and therefore more suitable for chokes.

    I didn't record all the results so far since most were pretty bad. Here is an example which I did happen to record. It approached 50% efficiency at some settings, but I'm not happy with it, so this core is ruled out. This was with a type T38 core (B64290L0044X038)

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to anniel747

    Do you mean component pulls? No, I'm trying to use easily-available parts, to make it repeatable. It's just unfortunate that most of the toroids I have (all with a part code so they can be purchased) are lossy, and therefore more suitable for chokes.

    I didn't record all the results so far since most were pretty bad. Here is an example which I did happen to record. It approached 50% efficiency at some settings, but I'm not happy with it, so this core is ruled out. This was with a type T38 core (B64290L0044X038)

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • anniel747
    anniel747 over 3 years ago in reply to shabaz

    You chose one labeled EM and you need one labeled Resonance (the ones that end by X001). 

    product.tdk.com/.../list

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to anniel747

    Hi! Totally agree, those are more suitable, but personally I'd have difficulty using those (too low AL value, I struggle beyond about 25-30 turns on a ferrite core, and I want to keep the frequency low too, since I'm only optimising for cost and noise (easier to reduce if it's lower). I've ordered some in-between materials, i.e. to tolerate some loss. 

    Incidentally, there's this excellent web page found by chance:

    https://neosid.com.au/ref-b.html

    Definitely worth bookmarking, it helped compare options, since some of the manufacturer parts have to be eliminated if some distributors are more preferred than others.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to shabaz

    Here are the candidates - I'll try some of these next week when they arrive.

    MPN Ferrite Type AL Dimensions mm
    Outer Inner Height Mech Type
    5977000301 77 1180 12.7 7.15 4.9 Toroid
    5977001101 77 1300 12.7 7.9 6.35 Toroid
    5977001801 77 1305 22.1 13.7 6.35 Toroid
    5977000601 77 1270 21 13.2 6.35 Toroid
    5977000621 77 1270 21.85 12.4 7.1 Toroid
    5977006401 77 2700 25.4 15.5 12.7 Toroid
    5961001801 61 75 22.1 13.7 6.35 Toroid
    5961001001 61 80 29 19 7.5 Toroid
    B64290L0045X049 N49 970 16 9.6 6.3 Toroid
    B64290L0719X049 N49 1130 22.1 13.7 7.9 Toroid
    B66413G0000X197 N97 820 Approx. 16x15x8 assembled EFD 15/8/5
    B66414W1008D1 - Bobbin
    B66414B2000X000 - Clip
    B66305G0000X187 N87 850 Approx. 16x15x9 assembled E 13/7/4 (EF 12.6)
    B66202B1108T001 - Bobbin
    B66202A2010X000 - Clip
    B66307G0000X187 N87 1000 Approx. 19x18x12 assembled E16/8/5 (EF 16)
    B66308B1108T001 - Bobbin
    B66308A2010X000 - Clip