Passive Components
  • Technologies
  • More
Passive Components
Forum Dealing with Unexpected Emissions: The Fellowship of the Ferrite Ring
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 107 subscribers
  • Views 6123 views
  • Users 0 members are here
  • ferrite ring
  • MXO4
  • emc
  • MXO 4
  • spectrum analyzer
  • toroid
  • choke
  • oscillator
  • ferrite core
  • Fair-Rite
  • ferrite
  • inductor
Related

Dealing with Unexpected Emissions: The Fellowship of the Ferrite Ring

shabaz
shabaz over 3 years ago


I was experimenting with bits of circuit, hopefully, to become a power supply eventually. It is a work in progress.

At this stage, I’m using bits of scrap copper-clad board, each with a sub-module. It’s too early for a PCB.

image

However, during the prototyping, I noticed (amongst other issues that I need to solve!) a particular artifact on the ‘scope trace when looking at the output.

This situation ended up being a good example of where it pays to zoom out and look at a lot more of the spectrum view than expected!

Admittedly this was a lot easier to identify using the MXO 4 ‘scope, but it would be possible to spot with other test equipment, such as a spectrum analyzer and a near-field probe. I just used the normal 'scope probe, I didn't do anything special.

With the MXO 4, the anomaly was zoomed in, and then using a logarithmic-frequency spectrum view, it was possible to see the extent of the problem, with the left side of the spectrum view showing the wanted oscillation (fundamental frequency) and its harmonics, and the right side showing the spurious output.

image

Now I could try to do something about it!

I used tiny ferrite rings (legend has it they were forged by Fair-Rite, part code 2643001501 ) on the base input of the transistors. Essentially, they act as a bit of additional resistance for the higher frequencies. The rings cost $0.02 currently (although more expensive in the UK).

image


Back to the ‘scope:

image

Much better!

As mentioned, I still have other problems to deal with, but I thought it was a nice example of why it makes sense to do testing to frequencies far higher than expected, just in case there are spurious emissions, and why it can be a good idea to possess the rings because one never knows when they are needed.

Thanks for reading!

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to anniel747 +3
    or nail polish. Also good to fix broken-off enamel.
  • robogary
    robogary over 3 years ago +2
    nice. I wouldnt have looked that closely to notice the ring.
  • anniel747
    anniel747 over 3 years ago in reply to shabaz +2
    Or conventional varnish dip.
Parents
  • shabaz
    shabaz over 3 years ago

    Here are some results for what I'm calling "Scenario A", which is needing a small negative supply rail for an op-amp, capable of 10 mA or so. For this test, I'm using a 5V power source.

    The ferrite was 5977001101 which is type 77. 

    At no load, the input current consumption is 10 mA, and the output looks pretty good (this is probing with a long ground clip, on the AC [i.e. unrectified] output).

    image

    With a schottky diode bridge rectifier, and about 15 uF of output capacitance, I see an output of 4.1V DC. 

    It is expected for the waveform to change shape with a load, that is a characteristic of this type of design. The design can be tweaked to try to make the waveform as best as possible at the desired load.

    With a  5 mA load, the output is about 3.2V. With a 10 mA load, the output is just slightly over 3.0V.

    Here is the AC waveform at the input of the bridge rectifier, at 5 mA load:

    image

    Here is the waveform at 10 mA load:

    image

    At the output of the bridge rectifier, at 10 mA load (this is with better probing than with the AC waveforms above):

    image

    Probably for non-critical stuff this could be used as-is, since there's not much ripple (about 10 mV), but an LDO could be used to remove that, and end up with (say) a 1V or 2V supply, capable of being a negative rail since it is currently isolated. TLV740 series would get rid of most of the remaining noise I think. It's also very low-cost!

    Total cost is under £2.30 ($3 USD) including the voltage regulator, assuming the approx 1.5 meters of enameled wire is free. 

    I'm thinking maybe I should document each scenario separately, otherwise it's going to be very easy to mix up the configurations and results.

    Maybe scenario "B" would be a supply rail that is equal to the input supply (e.g. if symmetrical supplies are needed for an op-amp, or if an isolated supply is needed for parts of circuitry).

    Scenario "C" could be a 3.3V to 5V, or 5V to 12V converter maybe!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    Here are some results for what I'm calling "Scenario A", which is needing a small negative supply rail for an op-amp, capable of 10 mA or so. For this test, I'm using a 5V power source.

    The ferrite was 5977001101 which is type 77. 

    At no load, the input current consumption is 10 mA, and the output looks pretty good (this is probing with a long ground clip, on the AC [i.e. unrectified] output).

    image

    With a schottky diode bridge rectifier, and about 15 uF of output capacitance, I see an output of 4.1V DC. 

    It is expected for the waveform to change shape with a load, that is a characteristic of this type of design. The design can be tweaked to try to make the waveform as best as possible at the desired load.

    With a  5 mA load, the output is about 3.2V. With a 10 mA load, the output is just slightly over 3.0V.

    Here is the AC waveform at the input of the bridge rectifier, at 5 mA load:

    image

    Here is the waveform at 10 mA load:

    image

    At the output of the bridge rectifier, at 10 mA load (this is with better probing than with the AC waveforms above):

    image

    Probably for non-critical stuff this could be used as-is, since there's not much ripple (about 10 mV), but an LDO could be used to remove that, and end up with (say) a 1V or 2V supply, capable of being a negative rail since it is currently isolated. TLV740 series would get rid of most of the remaining noise I think. It's also very low-cost!

    Total cost is under £2.30 ($3 USD) including the voltage regulator, assuming the approx 1.5 meters of enameled wire is free. 

    I'm thinking maybe I should document each scenario separately, otherwise it's going to be very easy to mix up the configurations and results.

    Maybe scenario "B" would be a supply rail that is equal to the input supply (e.g. if symmetrical supplies are needed for an op-amp, or if an isolated supply is needed for parts of circuitry).

    Scenario "C" could be a 3.3V to 5V, or 5V to 12V converter maybe!