Passive Components
  • Technologies
  • More
Passive Components
Forum Seeking Proposals for Capacitor, Inductor or Resistor Projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 115 subscribers
  • Views 4195 views
  • Users 0 members are here
  • passive_featured
Related

Seeking Proposals for Capacitor, Inductor or Resistor Projects

rscasny
rscasny over 8 years ago

I am looking to sponsor passive components projects. It can be anything involving capacitors, inductors or resistors.

 

If you are instrested, please offer your project ideas in the comments below. Also, give me a rough idea of the BOM.

 

Randall

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +7
    Hi Randall, I'm planning on making a single-reference resistor standard, but I've already purchased the bits and pieces.It uses a single precision resistor - I thought it would be useful to have around…
  • fmilburn
    fmilburn over 8 years ago +5
    Using supercapacitors to store energy and power project along the lines of the Solar Bubble Blaster project that I did. The circuit consists of capacitors and diodes. If you add diodes then there are a…
  • baldengineer
    baldengineer over 8 years ago +5
    Having worked at a capacitor company, I can suggest projects like these where the caps are, relatively speaking, critical. Or at least, they are not an after-thought. Power Banks Sometimes these are called…
Parents
  • actionkindaguy
    actionkindaguy over 8 years ago

    Hi Randall,

    I am working on an rfid chessboard project I designed utilizing 125 Khz rfid technology. The main chessboard, for each of the 64 squares, has passive components consisting of a coil and capacitor and fast switching diode. The chessboard scanning is accomplished by multiplexing a few active components, capacitors, and resistors and only requires a few GPIO pins from a micro controller (esp32). The micro controller takes care of deciphering the data stream, chessboard scanning, and signal generation. The micro controller really could be any out there but I wanted to utilize the built-in Bluetooth and wifi that comes with the esp32 later in the project.

    So far approx BOM:

    (64 1n4154 fast switching diodes

    (64) coils ~ 275 uH,

    (70) capacitors

    (15) resistors

    (1) LM324

    (4) 74hc4066

    (2) 74HC595

    (1) 2N7000

    (1) ESP32 sparkfun module

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • actionkindaguy
    actionkindaguy over 8 years ago

    Hi Randall,

    I am working on an rfid chessboard project I designed utilizing 125 Khz rfid technology. The main chessboard, for each of the 64 squares, has passive components consisting of a coil and capacitor and fast switching diode. The chessboard scanning is accomplished by multiplexing a few active components, capacitors, and resistors and only requires a few GPIO pins from a micro controller (esp32). The micro controller takes care of deciphering the data stream, chessboard scanning, and signal generation. The micro controller really could be any out there but I wanted to utilize the built-in Bluetooth and wifi that comes with the esp32 later in the project.

    So far approx BOM:

    (64 1n4154 fast switching diodes

    (64) coils ~ 275 uH,

    (70) capacitors

    (15) resistors

    (1) LM324

    (4) 74hc4066

    (2) 74HC595

    (1) 2N7000

    (1) ESP32 sparkfun module

    • Cancel
    • Vote Up +3 Vote Down