Passive Components
  • Technologies
  • More
Passive Components
Documents Audio Tweaker's Wishlist - What do I need to build/maintain audio gear?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dychen
  • Date Created: 10 Jan 2022 10:02 PM Date Created
  • Last Updated Last Updated: 28 Mar 2023 12:25 PM
  • Views 52341 views
  • Likes 12 likes
  • Comments 78 comments
Related
Recommended

Audio Tweaker's Wishlist - What do I need to build/maintain audio gear?

image

Many makers and engineers got into engineering through audio. Whether it be building a guitar pedal or modding the power amp in your home theater, working with audio components is a fun way to use your engineering skills.

This wishlist presents some of the tools and parts you need for working with audio. Audio is a broad topic, so this wishlist is a general overview of analog audio components. We'll get specific in later articles.

Tools
For audio related building, here are some handy tools to have on your bench!

Oscilloscope
An oscilloscope is your best friend for audio work. They can be used to check frequency response, distortion characteristics, and everything other specification that is important to an audio signal.

Oscilloscope

Multicomp Pro Oscilloscope

Function Generator
Audio work is all about frequencies. A function generator sends different kinds of waves at different frequencies so you know if your build is responding the way you want it to.

 Function Generator

Multicomp Pro Function Generator

Multimeter
Multimeters are essential for every kind of electronics work; audio is no different.

Multimeter

Multicomp Pro Multimeter

Speaker Dummy Load
Since we can't use speakers for our testing, all that power needs someplace to go. A dummy load simulates a speaker in your circuit without blowing your head off with volume. A dummy load can be built with a high wattage resistor at the desired resistance, usually 4, 8, or 16 ohms for speakers.

Speaker Dummy Load

Vishay Dummy Load

Contact Cleaner
If you're repairing equipment that has scratchy pots, many times, a bottle of contact cleaner is all you need. Drip a little bit into the pot and exercise it; your noise issues will often disappear.

Contact Cleaner

Contact Cleaner  

Helping Hands
You've probably already got a nice soldering station, so we won't get into soldering equipment, but with any soldering project, because we don't have six arms ourselves, a set of helping hands is very valuable.

Helping Hands

Duratool Helping Hands

Components
Audio circuits use a wide variety of analog components to keep that audio sounding good.

Transistors
Transistors are typically used to amplify audio signals, and sometimes distort. Different types of transistors have different characteristics, whether they are BJT, MOSFET, JFET, or even silicon or germanium.

Transistor

Multicomp Pro Transistor

Potentiometers
If you're putting any kind of analog controls on your new creation, you'll likely need pots or faders.

Potentiometer

Bourns Potentiometer

Opamps
Opamps (operational amplifier) designed to amplify signals and there's a wide range, from large and discrete, like the vintage API 2520 (and its descendants), to surface mount. Opamp design has come a long way and newer opamps, like the AD797, boast near zero distortion and noise, although classic opamps like the TL072 and 5532 still offer great sounds in the right circuit.

Opamp

AD797 Opamp

Transformers
Transformers do a whole lot of things in an audio circuit; impedance matching, balancing, stepping up or down, etc. Because they only transmit audio signals, transformers also provide an important benefit: isolation.

Transformer

Hammond 119DA Transformer

Power Supply
Your opamps and transistors need to be powered, so chances are you'll need a good DC power supply. Op amps typically take somewhere in the range of +/-16V, while a discrete transistor based circuit might require a 24V supply. If you're making a microphone preamp that supplies phantom power, you'll need to supply 48V.

Power Supply

Delta 24V Power Supply

Connectors
To get your audio signal in and out of your circuit, you'll need connectors.

 

XLR Connector

Neutrik XLR Connector

Terminal connectors

Cliff 8-Way Spring Terminal

Speakers, Headphones, and Mic
Now the fun part! The most important tools for testing audio devices are your ears.  Speakers, speaker drivers, and headphones are the most important tools once you're ready to test your design. Fingers crossed that you don't get a blast of loud feedback when you flip the switch!

Trust powered speakers

Trust Speakers

Headphones

Koss UR20 Headphones


There are several different types of microphones – large diaphragm condensers, small diaphragm condensers, dynamics, ribbons, and more, all designed for specific purposes. We’ve selected a lavalier because it’s a tiny inexpensive mic that is convenient for testing on the bench.

Microphone

Pulse Lavalier Microphone

  • Audio Giveaway
  • audio
  • Audio Tweakers
  • sound
  • music
  • Home Theater
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dychen
    dychen over 4 years ago +2
    Here's a shot of my studio. Forgive the mess...it's a work in progress. All the gear was collected over the years, sometimes not working. I repaired/recapped everything so that it's all working...well…
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to Jan Cumps +2
    I love tape.. hisss.
  • robogary
    robogary over 4 years ago +2
    Lets have a hearty cheer for one of our best friends in building analog audio circuits - the DC blocking capacitor ! HEAR ! HEAR ! :-) My other dear friend is the audio transformer. I actually use Midcom…
Parents
  • phoenixcomm
    phoenixcomm over 4 years ago

    imageI have been messing around with audio since high school. My first good amp was a Dynaco stereo 70. I had new tubes and caps put in 1976. The current list of junk is (top-down):

    • Technics SL2000 Turntable w/ Stanton 681EEE Ref Standard.
    • Moster power Control 5000 ( it gets power but will not turn on. MOR TO FIX.
    • Phase Linear 5000 FM Tuner
    • Yamaha DSR-100PRO Surround Sound Decoder
    • Sony  TA-E100 Control amp (preamp) 
    • DIY stereo preamp for the 681EEE Cart
    • Sony Disk Player DVP-NS900
    • Sony Quad Amp N220
    • Speakers pair of Bose 201s 
    • Klipsch SUB-10 (No amp) hard wired to N220)
    • Klipsch KV-1 Center Chanel 


    Flow is a little crazy after Control amp -> Surround Sound Decoder the Sony Quad amp which goes to:

    • bose Left front
    • Klipsch Center
    • Klipsch Sub
    • Bose right
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to phoenixcomm

    I bought this one this week, second hand. I have it from yesterday. I used to play CDs from my laptop. I won a new laptop with a design contest here (yay!). But these days they come without a CD player. So I lookedfor a decentone for sale in the neighbourhood.

    image

    Other elements, more or les in permanent use (the record player has been featured in a repair blog here):

    image

    image

    image

    Everything has had at least one previous owner.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to phoenixcomm

    I bought this one this week, second hand. I have it from yesterday. I used to play CDs from my laptop. I won a new laptop with a design contest here (yay!). But these days they come without a CD player. So I lookedfor a decentone for sale in the neighbourhood.

    image

    Other elements, more or les in permanent use (the record player has been featured in a repair blog here):

    image

    image

    image

    Everything has had at least one previous owner.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to Jan Cumps

    yes, most of mine came from pawn shops! the only three pieces that I bought when new on a clearance  FM tuner,  The SS Decoder was new and the turntable was new. and the Stanton Cartridge it was a little more than 100 bucks way back in 76 when I worked for Interdata. so the cost of ownership is about 50 cents a year. I just had to repoint the needle say $80.00 so the TCO is less than 1 dollar a year. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    Forgot oneimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to Jan Cumps

    I love tape.. hisss. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to phoenixcomm

    Hehe. And this one has that. It's a version without any noise reduction.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to Jan Cumps

    NAD stuff always looks nice and understated : ) I have a NAD receiver, bought used maybe 10 years ago, but it is over 20 years old, and it is not replaceable (not that I would want to!) because FM receiver quality has gone significantly backward since then. It's easy to forget you're listening to a radio station and not tape/disc, until the presenter interrupts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dychen
    dychen over 4 years ago in reply to Jan Cumps

    Love it! I wish I had a 2-track reel to reel.  Mine's a 16 track (Tascam MS-16)...it just sits there gathering dust now. I'm trying to think of ways to get it back into use, but tape is a little expensive these days.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to dychen

    This is the one I had, in the 1st half of the 90's: Teac 80-8
    image

    image source: www.hifiengine.com/.../teac-80-8.shtml-0

    Without the DB-x unit shown at the bottom, but with speed control unit.
    1/2" tape and the NAB type spools were still available at the time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to Jan Cumps

    imageThis is what I used to have Roberts 700x. The knob with the X on it changed the recording modes.

    image from eBay.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dychen
    dychen over 4 years ago in reply to Jan Cumps

    Very nice!  Mine also doesn't have dbx...it's set to run at 30ips so noise reduction isn't an issue, but I would like to try 15ips on it at some point.